Maintenance license (1 year) for the SUP-1 Emalytics Supervisor license
Rakennusten hallintajärjestelmä
Emalytics-rakennustenhallintajärjestelmämme tarjoaa alustan rakennuksesi kaikille digitaalisen infrastruktuurin keskeisille elementeille. Emalytics yhdistää hallinta- ja käyttölaitteiston sekä energianvalvonnan yhteen älykkääseen alustaan. IoT-pohjaisen kehyksen avulla voit hallita, analysoida ja käsitellä kaikkien osajärjestelmien tietoja ja informaatiota tarpeen mukaan. Hyödy suunnittelun helppoudesta ja yhdestä alustasta rakennuksen kaikkia prosesseja ja sovelluksia varten.
Maintenance license (1 year) for the Emalytics Controller license NC4-10000
Upgrade license for Emalytics View to extend the runtime license from 500 Niagara data points to 25000 data points; this license has no time limit.
Please note that the following information must be provided when purchasing this license: The host ID of the machine on which Emalytics View is running and the email address to which the license is to be sent.
Upgrade license for Emalytics View to extend the runtime license from 5000 Niagara data points to an unlimited number of data points; this license has no time limit.
Please note that the following information must be provided when purchasing this license: The host ID of the machine on which Emalytics View is running and the email address to which the license is to be sent.
Maintenance license (1 year) for the SUP-0 Emalytics Supervisor license
Maintenance license (3 years) for the Emalytics Controller license NC4-5000
Upgrade license for Emalytics View to extend the runtime license from 250 Niagara data points to 1250 data points; this license has no time limit.
Please note that the following information must be provided when purchasing this license: The host ID of the machine on which Emalytics View is running and the email address to which the license is to be sent.
Upgrade license for Emalytics View to extend the runtime license from 250 Niagara data points to an unlimited number of data points; this license has no time limit.
Please note that the following information must be provided when purchasing this license: The host ID of the machine on which Emalytics View is running and the email address to which the license is to be sent.
Upgrade license for Emalytics View to extend the runtime license from 5000 Niagara data points to 50000 data points; this license has no time limit.
Please note that the following information must be provided when purchasing this license: The host ID of the machine on which Emalytics View is running and the email address to which the license is to be sent.
Upgrade license for Emalytics View to extend the runtime license from 1250 Niagara data points to 50000 data points; this license has no time limit.
Please note that the following information must be provided when purchasing this license: The host ID of the machine on which Emalytics View is running and the email address to which the license is to be sent.