Upgrade license for Emalytics View to extend the runtime license from 500 Niagara data points to 5000 data points; this license has no time limit.
Please note that the following information must be provided when purchasing this license: The host ID of the machine on which Emalytics View is running and the email address to which the license is to be sent.
Rakennusten hallintajärjestelmä
Emalytics-rakennustenhallintajärjestelmämme tarjoaa alustan rakennuksesi kaikille digitaalisen infrastruktuurin keskeisille elementeille. Emalytics yhdistää hallinta- ja käyttölaitteiston sekä energianvalvonnan yhteen älykkääseen alustaan. IoT-pohjaisen kehyksen avulla voit hallita, analysoida ja käsitellä kaikkien osajärjestelmien tietoja ja informaatiota tarpeen mukaan. Hyödy suunnittelun helppoudesta ja yhdestä alustasta rakennuksen kaikkia prosesseja ja sovelluksia varten.
Emalytics Niagara Cloud Service Remote annual subscription for the supervisor (separate maintenance license required)
Maintenance license (3 years) for the Emalytics Controller license NC4-100
Maintenance license (1 year) for the NC4-50 Emalytics Controller license
Runtime license for Emalytics View for the visualization of an unlimited number of Niagara data points; this license has no time limit.
Please note that the following information must be provided when purchasing this license: The host ID of the machine on which Emalytics View is running and the email address to which the license is to be sent.
Upgrade license for Emalytics View to extend the runtime license from 2500 Niagara data points to 50000 data points; this license has no time limit.
Please note that the following information must be provided when purchasing this license: The host ID of the machine on which Emalytics View is running and the email address to which the license is to be sent.
Upgrade license for Emalytics View to extend the runtime license from 1250 Niagara data points to 10000 data points; this license has no time limit.
Please note that the following information must be provided when purchasing this license: The host ID of the machine on which Emalytics View is running and the email address to which the license is to be sent.
Maintenance license (5 years) for the Emalytics Controller license NC4-10000
Emalytics Supervisor license with connectivity to any number of Emalytics Controllers (separate maintenance license required)
Emalytics Controller license to integrate 1250 data points (separate maintenance license required)