Emalytics Supervisor license for CSV database driver
Rakennusten hallintajärjestelmä
Emalytics-rakennustenhallintajärjestelmämme tarjoaa alustan rakennuksesi kaikille digitaalisen infrastruktuurin keskeisille elementeille. Emalytics yhdistää hallinta- ja käyttölaitteiston sekä energianvalvonnan yhteen älykkääseen alustaan. IoT-pohjaisen kehyksen avulla voit hallita, analysoida ja käsitellä kaikkien osajärjestelmien tietoja ja informaatiota tarpeen mukaan. Hyödy suunnittelun helppoudesta ja yhdestä alustasta rakennuksen kaikkia prosesseja ja sovelluksia varten.
Upgrade of the Emalytics Supervisor license for connectivity to an additional Emalytics Controller (it is possible to use several update licenses to integrate more than one additional controller).
Runtime license for Emalytics View for the visualization of up to 500 Niagara data points; this license has no time limit.
Please note that the following information must be provided when purchasing this license: The host ID of the machine on which Emalytics View is running and the email address to which the license is to be sent.
Emalytics Controller license for an additional 2500 data points
Runtime license for Emalytics View for the visualization of up to 50000 Niagara data points; this license has no time limit.
Please note that the following information must be provided when purchasing this license: The host ID of the machine on which Emalytics View is running and the email address to which the license is to be sent.
Upgrade of Emalytics Supervisor license from SUP-100 to connectivity to any number of Emalytics Controllers (SUP-UNL)
Emalytics Supervisor license for an additional 1250 data points
Upgrade license for Emalytics View to extend the runtime license from 2500 Niagara data points to 10000 data points; this license has no time limit.
Please note that the following information must be provided when purchasing this license: The host ID of the machine on which Emalytics View is running and the email address to which the license is to be sent.
Maintenance license (3 years) for the SUP-1 Emalytics Supervisor license
Runtime license for Emalytics View for the visualization of up to 25000 Niagara data points; this license has no time limit.
Please note that the following information must be provided when purchasing this license: The host ID of the machine on which Emalytics View is running and the email address to which the license is to be sent.