Runtime license for Emalytics View for the visualization of up to 2500 Niagara data points; this license has no time limit.
Please note that the following information must be provided when purchasing this license: The host ID of the machine on which Emalytics View is running and the email address to which the license is to be sent.
Rakennusten hallintajärjestelmä
Emalytics-rakennustenhallintajärjestelmämme tarjoaa alustan rakennuksesi kaikille digitaalisen infrastruktuurin keskeisille elementeille. Emalytics yhdistää hallinta- ja käyttölaitteiston sekä energianvalvonnan yhteen älykkääseen alustaan. IoT-pohjaisen kehyksen avulla voit hallita, analysoida ja käsitellä kaikkien osajärjestelmien tietoja ja informaatiota tarpeen mukaan. Hyödy suunnittelun helppoudesta ja yhdestä alustasta rakennuksen kaikkia prosesseja ja sovelluksia varten.
Maintenance license (1 year) for the Emalytics Controller license NC4-1250
Emalytics Niagara Cloud Service Recover annual subscription for a controller (separate maintenance license required)
Emalytics Controller license for an additional 50 data points
Maintenance license (3 years) for SUP-0 Emalytics Supervisor license
Emalytics Supervisor license for an additional 5000 data points
Upgrade license for Emalytics View to extend the runtime license from 250 Niagara data points to 25000 data points; this license has no time limit.
Please note that the following information must be provided when purchasing this license: The host ID of the machine on which Emalytics View is running and the email address to which the license is to be sent.
SMS driver license for Emalytics Controller
Upgrade license for Emalytics View to extend the runtime license from 250 Niagara data points to 2500 data points; this license has no time limit.
Please note that the following information must be provided when purchasing this license: The host ID of the machine on which Emalytics View is running and the email address to which the license is to be sent.
Upgrade license for Emalytics View to extend the runtime license from 250 Niagara data points to 5000 data points; this license has no time limit.
Please note that the following information must be provided when purchasing this license: The host ID of the machine on which Emalytics View is running and the email address to which the license is to be sent.