Maintenance license (5 years) for the NC4-50 Emalytics Controller license
Sistema de gestão de edifícios
Com o sistema de gestão de edifícios Emalytics oferecemos-lhe uma plataforma para todos os elementos centrais da infraestrutura digital do seu edifício. O Emalytics reúne numa plataforma inteligente o sistema de gestão e operação, bem como a monitorização de energia. Com a estrutura baseada na IoT, é possível controlar, avaliar e processar os dados e as informações de todas as unidades parciais, em função da necessidade. Beneficie de uma engenharia simples e de uma plataforma para todos os processos e aplicações no seu edifício.
Emalytics Controller license for an additional 500 data points
Upgrade license for Emalytics View to extend the runtime license from 500 Niagara data points to an unlimited number of data points; this license has no time limit.
Please note that the following information must be provided when purchasing this license: The host ID of the machine on which Emalytics View is running and the email address to which the license is to be sent.
Maintenance license (1 year) for the Emalytics Controller license NC4-10000
Upgrade license for Emalytics View to extend the runtime license from 500 Niagara data points to 25000 data points; this license has no time limit.
Please note that the following information must be provided when purchasing this license: The host ID of the machine on which Emalytics View is running and the email address to which the license is to be sent.
Upgrade license for Emalytics View to extend the runtime license from 5000 Niagara data points to an unlimited number of data points; this license has no time limit.
Please note that the following information must be provided when purchasing this license: The host ID of the machine on which Emalytics View is running and the email address to which the license is to be sent.
Maintenance license (1 year) for the SUP-0 Emalytics Supervisor license
Maintenance license (3 years) for the Emalytics Controller license NC4-5000
Upgrade license for Emalytics View to extend the runtime license from 250 Niagara data points to 1250 data points; this license has no time limit.
Please note that the following information must be provided when purchasing this license: The host ID of the machine on which Emalytics View is running and the email address to which the license is to be sent.
Upgrade license for Emalytics View to extend the runtime license from 250 Niagara data points to an unlimited number of data points; this license has no time limit.
Please note that the following information must be provided when purchasing this license: The host ID of the machine on which Emalytics View is running and the email address to which the license is to be sent.