Runtime license for Emalytics View for the visualization of up to 25000 Niagara data points; this license has no time limit.
Please note that the following information must be provided when purchasing this license: The host ID of the machine on which Emalytics View is running and the email address to which the license is to be sent.
Sistema de gestão de edifícios
Com o sistema de gestão de edifícios Emalytics oferecemos-lhe uma plataforma para todos os elementos centrais da infraestrutura digital do seu edifício. O Emalytics reúne numa plataforma inteligente o sistema de gestão e operação, bem como a monitorização de energia. Com a estrutura baseada na IoT, é possível controlar, avaliar e processar os dados e as informações de todas as unidades parciais, em função da necessidade. Beneficie de uma engenharia simples e de uma plataforma para todos os processos e aplicações no seu edifício.
Maintenance license (1 year) for the SUP-100 Emalytics Supervisor license
Emalytics Supervisor license without connectivity to an Emalytics Controller (separate maintenance license required)
Upgrade license for Emalytics View to extend the runtime license from 1250 Niagara data points to an unlimited number of data points; this license has no time limit.
Please note that the following information must be provided when purchasing this license: The host ID of the machine on which Emalytics View is running and the email address to which the license is to be sent.
Emalytics Supervisor license for SQL database driver
Emalytics Supervisor license for an additional 500 data points
Access to the Emalytics Automation license portal for 1 year (May 1 - April 30).
Enables you to view, download, and move Emalytics Automation licenses. It is not possible to purchase new licenses independently. The order must still be placed via your Phoenix Contact sales team.
The actual total billing amount is calculated based on the remaining period through to April 30.