Runtime license for Emalytics View for the visualization of an unlimited number of Niagara data points; this license has no time limit.
Please note that the following information must be provided when purchasing this license: The host ID of the machine on which Emalytics View is running and the email address to which the license is to be sent.
Sistema de gestão de edifícios
Com o sistema de gestão de edifícios Emalytics oferecemos-lhe uma plataforma para todos os elementos centrais da infraestrutura digital do seu edifício. O Emalytics reúne numa plataforma inteligente o sistema de gestão e operação, bem como a monitorização de energia. Com a estrutura baseada na IoT, é possível controlar, avaliar e processar os dados e as informações de todas as unidades parciais, em função da necessidade. Beneficie de uma engenharia simples e de uma plataforma para todos os processos e aplicações no seu edifício.
Upgrade license for Emalytics View to extend the runtime license from 2500 Niagara data points to 50000 data points; this license has no time limit.
Please note that the following information must be provided when purchasing this license: The host ID of the machine on which Emalytics View is running and the email address to which the license is to be sent.
Upgrade license for Emalytics View to extend the runtime license from 1250 Niagara data points to 10000 data points; this license has no time limit.
Please note that the following information must be provided when purchasing this license: The host ID of the machine on which Emalytics View is running and the email address to which the license is to be sent.
Maintenance license (5 years) for the Emalytics Controller license NC4-10000
Emalytics Supervisor license with connectivity to any number of Emalytics Controllers (separate maintenance license required)
Upgrade license for Emalytics View to extend the runtime license from 250 Niagara data points to 10000 data points; this license has no time limit.
Please note that the following information must be provided when purchasing this license: The host ID of the machine on which Emalytics View is running and the email address to which the license is to be sent.
Emalytics Controller license to integrate 50 data points (separate maintenance license required)
Runtime license for Emalytics View for the visualization of up to 250 Niagara data points; this license has no time limit.
Please note that the following information must be provided when purchasing this license: The host ID of the machine on which Emalytics View is running and the email address to which the license is to be sent.
Emalytics Supervisor license with connectivity to up to 10 Emalytics Controllers (separate maintenance license required)
Upgrade license for Emalytics View to extend the runtime license from 10000 Niagara data points to 25000 data points; this license has no time limit.
Please note that the following information must be provided when purchasing this license: The host ID of the machine on which Emalytics View is running and the email address to which the license is to be sent.