Maintenance license (3 years) for the Emalytics Controller license NC4-500
Sistema de gestão de edifícios
Com o sistema de gestão de edifícios Emalytics oferecemos-lhe uma plataforma para todos os elementos centrais da infraestrutura digital do seu edifício. O Emalytics reúne numa plataforma inteligente o sistema de gestão e operação, bem como a monitorização de energia. Com a estrutura baseada na IoT, é possível controlar, avaliar e processar os dados e as informações de todas as unidades parciais, em função da necessidade. Beneficie de uma engenharia simples e de uma plataforma para todos os processos e aplicações no seu edifício.
Maintenance license (5 years) for the Emalytics Controller license NC4-250
Emalytics Supervisor license for CSV database driver
Runtime license for Emalytics View for the visualization of up to 500 Niagara data points; this license has no time limit.
Please note that the following information must be provided when purchasing this license: The host ID of the machine on which Emalytics View is running and the email address to which the license is to be sent.
Emalytics Controller license for an additional 2500 data points
Runtime license for Emalytics View for the visualization of up to 50000 Niagara data points; this license has no time limit.
Please note that the following information must be provided when purchasing this license: The host ID of the machine on which Emalytics View is running and the email address to which the license is to be sent.
Upgrade of Emalytics Supervisor license from SUP-100 to connectivity to any number of Emalytics Controllers (SUP-UNL)
Emalytics Supervisor license for an additional 1250 data points
Upgrade license for Emalytics View to extend the runtime license from 2500 Niagara data points to 10000 data points; this license has no time limit.
Please note that the following information must be provided when purchasing this license: The host ID of the machine on which Emalytics View is running and the email address to which the license is to be sent.
Maintenance license (3 years) for the SUP-1 Emalytics Supervisor license