Upgrade license for Emalytics View to extend the runtime license from 2500 Niagara data points to 5000 data points; this license has no time limit.
Please note that the following information must be provided when purchasing this license: The host ID of the machine on which Emalytics View is running and the email address to which the license is to be sent.
Sistema de gestão de edifícios
Com o sistema de gestão de edifícios Emalytics oferecemos-lhe uma plataforma para todos os elementos centrais da infraestrutura digital do seu edifício. O Emalytics reúne numa plataforma inteligente o sistema de gestão e operação, bem como a monitorização de energia. Com a estrutura baseada na IoT, é possível controlar, avaliar e processar os dados e as informações de todas as unidades parciais, em função da necessidade. Beneficie de uma engenharia simples e de uma plataforma para todos os processos e aplicações no seu edifício.
Niagara Catan controller for 1250 data points (requires NC4-1250-SMA-XXX maintenance)
Emalytics Niagara Cloud Service Recover annual subscription for the supervisor (separate maintenance license required)
Emalytics Supervisor license for MYSQL database driver
Upgrade license for Emalytics View to extend the runtime license from 10000 Niagara data points to 50000 data points; this license has no time limit.
Please note that the following information must be provided when purchasing this license: The host ID of the machine on which Emalytics View is running and the email address to which the license is to be sent.
Maintenance license (5 years) for SUP-0 Emalytics Supervisor license
Maintenance license (1 year) for the SUP-10 Emalytics Supervisor license
Emalytics Controller license to integrate 100 data points (separate maintenance license required)
Upgrade license for Emalytics View to extend the runtime license from 5000 Niagara data points to 25000 data points; this license has no time limit.
Please note that the following information must be provided when purchasing this license: The host ID of the machine on which Emalytics View is running and the email address to which the license is to be sent.
Upgrade license for Emalytics View to extend the runtime license from 2500 Niagara data points to an unlimited number of data points; this license has no time limit.
Please note that the following information must be provided when purchasing this license: The host ID of the machine on which Emalytics View is running and the email address to which the license is to be sent.