The content you are viewing is tailored for Global. View Content for United States | Choose Another Country

Improved safety with line fault monitoring

2025-04-22
Resistor network for proximity switches with MINI Analog Pro isolation switch amplifier

On the basis of the new resistor network from Phoenix Contact, floating contacts and proximity switches can be used in combination with input modules in accordance with NAMUR IEC/EN 60947-5-6 for line fault monitoring. This proves to be indispensable in applications with high safety requirements.

Push-in Technology enables the resistor network to be integrated quickly and easily into existing cabling setups. The compact housing enables flexible installation, even in confined areas such as in cable ducts or small transmitter housings. With the Simple Apparatus declaration for simple equipment that is not a source of ignition, the resistor network is also suitable for use in potentially explosive environments.

The practical and efficient solution for line fault monitoring is ideal for retrofitting and improving safety in industrial applications.

Press Contact
Eva von der Weppen
Eva von der Weppen | Corporate Communications