The content you are viewing is tailored for Global. View Content for United States | Choose Another Country

Intelligent sector coupling in Bremerhaven, Germany A complete value-added chain for green hydrogen has been realized in the HY.City.Bremerhaven. Innovative automation technology ensures reliable sector coupling and a secure remote connection.

Hydrogen service station in the HY.City.Bremerhaven

Customer profile


Site overview of the production plants for the HY.City.Bremerhaven

Lighthouse project for green hydrogen in the HY.City.Bremerhaven

The production of green hydrogen is part of the regional hydrogen ecosystem of the HY.City.Bremerhaven. The project is considered a lighthouse when switching from fossil fuels to regenerative fuels. GP Joule, a system provider for integrated energy solutions, is the general contractor for the green hydrogen project of HY.City.Bremerhaven GmbH & Co. KG. As a part of this, GP Joule has realized a complete value-added chain for green hydrogen. It starts with electrolysis as a key technology and includes compression and storage in mobile tankers. The concept also includes a service station and suitable fuel cell buses for public transport. Only the wind turbine generator was already in place on the Grauwallring industrial estate. The generator is used as an energy supplier for the electrolyzer.

The challenge


Hydrogen trailers for intelligent hydrogen transport

Optimal power supply

Solutions were examined that provide the right type of energy in the required quantity at the optimum location at the right time. With the HyRunner, GP Joule has developed a mobile storage system that enables intelligent hydrogen transport from the electrolysis site to the service station or to industrial customers. The hydrogen trailers are a central component of the process chain. The vehicles include comprehensive control and interface intelligence. It had to be ensured that the explosion protection risk assessment did not limit the entire automation concept to expensive Ex components. In addition, it also had to be possible to transfer the data generated to a cloud, store it, and use it in a variety of ways.

The hydrogen service station autonomously supplies the hydrogen-based public transport system in Bremerhaven. From the perspective of digitalization, the HyRunner had to fit seamlessly into the digital process chain. Furthermore, the technical equipment for the data logistics must ensure a high level of availability.

The solution


With innovative automation technology to intelligent sector coupling

Learn more in the video about our solution for controlling hydrogen production locations and controlling the intelligent hydrogen trailers.

Automation kit for the Ex and non-Ex area
Control cabinet with cellular router and HMI
Control cabinet with PLCnext Control
Automation kit for the Ex and non-Ex area

One functional modular system economically covers both Ex and non-Ex areas. In the control cabinet, only processes from the Axioline product family are equipped with Ex I/O modules in which Ex protection is actually required. For example, input cards are used in the HyRunner for the valves of the hydrogen lines. They can be used to wire the signals directly to the correspondingly certified I/O modules. Separate Ex barriers are therefore superfluous or are only used where separate I/O modules would not be economical due to very few signal types. This saves valuable space and reduces costs. Outside of the Ex zone, the standard I/O portfolio from the Axioline modular system is sufficient, without functional limitations for a consistent overall system.

Control cabinet with cellular router and HMI

Data is transmitted to the cloud via an industrial cellular router from the TC Router 3002T-4G series installed in the control cabinet. The TC MGUARD RS4000 router provides the necessary IT and OT security. With this equipment, the roadworthy system can communicate independently and securely with the cloud. In addition, it enables time-efficient refueling in coordination with the upstream electrolysis and storage processes. For example, it enables fill volumes to be determined, valves to be controlled, and the current location of the trailer to be determined via GPS. The functions are supplemented by a system integrated into the PLCnext Control for the calibration-law compliant billing of the supplied hydrogen.

At the location of the electrolyzers, PLCnext Control is used as the highest control instance. This so-called location controller acquires all operating data of the process chain, from electrolysis through to the tank trailers. This data is forwarded wirelessly to a central evaluation unit via the TC MGUARD router and an antenna.

Control cabinet with PLCnext Control

Two QUINT4-PS-type power supplies in combination with a redundancy module from the QUINT O-ring product family ensure failsafe performance. The solution is supported by five battery modules, which together with a QUINT4-UPS form an uninterruptible power supply. In this way, short-term power failures can be bridged or the entire system can be shut down in a controlled manner in the event of a malfunction. This prevents the system from reaching a critical state due to the high reactivity of hydrogen. The two control units also create a high-availability redundancy pair via the concept of applicative system redundancy (ASR). The availability solution is rounded off by the network. This connects the individual submodules of the location to each other and, due to its ring structure, is failsafe against individual faults.

Contact

Your contact person, Andreas Lautmann
Andreas Lautmann
Business Development Manager, Power-to-X
“I would be happy to help you on your way to a carbon-neutral future with green hydrogen”.

Products


Discussion next to the control cabinet with automation technology in the HY.City.Bremerhaven

Still haven’t found the right product?

Feel free to contact us. Together, we can find an ideal solution for equipping your control cabinets with more than 100,000 products from the fields of connection, communication, and automation technology.

Summary


Partnership for the regional hydrogen ecosystem of HY.City.Bremerhaven

Maximum availability and safety in hydrogen infrastructure

Hydrogen production and tank infrastructure are part of the core concept of GP Joule. The locations are equipped with independent control technology, autonomously automated, and able to communicate with the higher-level cloud intelligence of GP Joule on both sides. For maximum availability, redundant controller hardware has been integrated, which is coordinated by the ASR (Applicative System Redundancy) smart software solution. In the face of the increasing risk of cyberattacks, comprehensive security solutions were also integrated. The use of MGUARD remote maintenance routers ensures secure communication within the hydrogen ecosystem. Hydrogen trailers play a central role as mobile storage and transport tanks. Explosion protection was integrated cost-effectively using one functional modular system that covers Ex and non-Ex areas.

This project is an impressive demonstration that solutions and technologies needed to realize an All Electric Society are already available.

You may also be interested in