The content you are viewing is tailored for Global. View Content for United States | Choose Another Country

Smooth lock operation on the Kiel Canal As part of modernization work, the lock system in Kiel’s Holtenau district has been equipped with a new signal system. The signal lights are designed to withstand harsh weather conditions and ensure secure communication with the power connection point.

Lock system in Kiel-Holtenau, Germany

Modernization of the lock system in Kiel-Holtenau

Customer profile


Employee at the Kiel Canal in Kiel

Kiel Canal, Kiel-Holtenau

The Kiel Canal connects the mouth of the Elbe with the Kiel Fjord, saving the ships a detour of up to 460 km. The approximately 100-kilometer-long waterway runs across Schleswig-Holstein and is one of the busiest artificial shipping routes in the world.

The challenge


Mast with signal lights

Harsh ambient conditions and necessary monitoring

As part of modernization work, the lock system in Kiel’s Holtenau district has been equipped with a new signaling system. The lights are installed on masts and use red, green, and white signals to notify approaching vessels of whether or not the lock entrance is unobstructed.

Only components that conform to the industry standard are used for the monitoring functions. The signal lights are exposed to harsh weather conditions and must therefore satisfy special requirements. These include high winds, salt water, and even direct sunlight.

The use of modern industrial communication technology ensures that the control room is always informed of the status of the lights. Easy installation without having to set addresses or device IDs is also desirable for maintenance crews. This is particularly important when lights have to be replaced for maintenance.

Solution


Service personnel accessing mobile operating data

Easy installation and transparent system states

Two new masts in the lock have been fitted with 300 LED signal lights, providing status and diagnostic information to support maintenance personnel. This is made possible with the use of industrial communication technology.

The lights are connected using pre-assembled cables and M17 hybrid connectors from Phoenix Contact. The hybrid connector simultaneously connects the power supply and the data cable to the light. There is no risk of mismatching. Easy installation is particularly important when lights have to be replaced for maintenance. This is where the benefits of an electronic rating plate that can be read via the communication link come into play. In this way, the control unit can detect whether the correct light is connected.

The color, size, and beam angle are transmitted, for example. In the event of faulty installation or replacement, the control unit sends an alarm message and prevents the light from turning itself on. The light’s operating hours and the those of the individual LEDs are recorded separately and stored cyclically in the light.

Signal lights system operation with LED technology

More energy-efficient system operation with LED technology

The LED technology in the light helps save energy and increase availability. The latter is a result not only of the extended service life, but also the special wiring of the lights.

When one LED fails, this is detected by a current and voltage monitoring system and reported back to the higher level system. According to the instructions from the control system, the other LEDs can be readjusted in order to achieve the same light output.

In addition to the LED monitoring, two scattered-light sensors are installed in the signal light, which detect whether the LEDs are emitting light as well as the intensity.

The temperature of the light is also recorded in order to ensure the operational safety of the signal light in all instances. If the temperature of the light exceeds the permissible range, light output is reduced or even switched off. This function is supported by notification and alarm messages. If the temperature drops again, the light resumes operation once the message has been acknowledged.

Your advantages

  • Seawater-resistant signal lamps with energy-saving LED technology
  • Simpler maintenance through support with status and diagnostic information
  • Easy installation with preassembled cables and connectors

Contact

Fabian Pasimeni
Fabian Pasimeni
Global Industry Manager Urban Infrastructure
I would be happy to provide the support you need in projects geared toward increasing traffic safety for locks, movable bridges, and gates.

Products


Person using a tablet in front of a control cabinet

Still haven’t found the right product?

Feel free to contact us. We will consult with you to find the ideal solution together.

Summary


Changing signal lights for waterways

Smooth operation and efficient processes

The locks, which compensate for the difference in level of the North Sea and Baltic Sea, play a central role in the smooth operation of the Kiel Canal. Lock maintenance is simplified by LED signal lights from Phoenix Contact, because their operating data can be read at anytime.

Maintenance personnel are supported with status and diagnostic information and are therefore continuously informed of the status of the signal lights. A further advantage of the lights is the LED technology that helps save energy and increase availability.