The content you are viewing is tailored for Global. View Content for United States | Choose Another Country

Extensions for ICS and ME-IO DIN rail connectors

2024-02-20
Connectors for DIN rail connectors

With the ME-IO and ICS housing series, Phoenix Contact offers a comprehensive portfolio for device development. The new extension items for the DIN rail connectors make it even easier to implement an entire system consisting of several modules.

Some applications also require data and signals from the module communication beyond the module network, for example, in the case of a line feed. Here, input and output connectors for the eight-position DIN rail connector connect modules over several levels. These connectors can be inserted into the device group on the left, in the middle, and on the right. The positions in the field are cabled via the FMC connector.

The transmission of data and signals for device applications without a necessary output to the PCB can be looped through by a bridge for DIN rail connectors below the module. This means that the maximum PCB surface is used.

Press Contact
Eva von der Weppen
Eva von der Weppen | Corporate Communications