The content you are viewing is tailored for Global. View Content for United States | Choose Another Country

Connectors with Push-in Technology

2024-11-12
Connexis connectors with Push-in Technology

The new Connexis DD31PS connectors with Push-in connection technology from Phoenix Contact simplify and accelerate wiring in the field and in the factory.

The trend towards preassembled solutions in industrial manufacturing offers companies the opportunity to make production processes faster and more efficient. However, there are also connections for various applications in the field that have to be wired on site by a specialist.
Here, the Push-in connection technology of the new wire-to-board connectors enables the flexible connection of components that are not preassembled. Thanks to the tool-free direct-connection technology, Push-in simplifies the wiring of rigid and flexible conductors with ferrules. To prevent mismatching, Phoenix Contact also provides coded connectors and headers.
With its various designs and versions, the DD31PS series is suitable for numerous applications, such as flying leads and panel feed-throughs. For example, in robotics, elevator technology, and battery management. The wire-to-board connectors with Push-in connection are available as double-row versions with 4 to 20 positions with a pitch of 3.81 mm. They complement the existing portfolio of wire-to-board connectors with crimp connection technology.

Press Contact
Eva von der Weppen
Eva von der Weppen | Corporate Communications