The content you are viewing is tailored for Global. View Content for United States | Choose Another Country

MTP DESIGNER Short times-to-market and a high degree of flexibility: MTP-compliant modules can be created quickly and easily with the MTP DESIGNER.

Person sitting at a computer creating MTP-compliant modules

The challenge


Creation

Increasing complexity and requirements

In a constantly changing world, system operators and system integrators, for example, are increasingly faced with short-term, variable customer requirements. Accordingly, production systems must be adapted to the required market requirements within a short time.
With Module Type Package (MTP), users benefit from a high degree of flexibility in the modularization of systems. Resources can also be conserved because of the reusability of the modules. However, automating modules requires a lot of time, and integrating them into the POL is very complex. In times of a shortage of skilled workers, it is becoming increasingly difficult to find the respective specialists. Due to the high degree of manual intervention needed in the module creation process, the chance of errors increases.

The solution


MTP DESIGNER logo with screen in the background

Engineering made easy with the MTP DESIGNER

The MTP DESIGNER is a module engineering tool that enables the easy and time-saving realization of modules in a processing plant.

To this end, P&IDs can be automatically imported from process engineering tools and a program body, and services for module automation can be generated. Modules are engineered based on this. The modules are generated in accordance with the VDI/VDE/NAMUR 2658 standard.
In parallel to this, the local visualization on the controller is automatically generated based on the P&ID and, at the same time, all interfaces (OPC UA tags) are defined for later data transfer. The MTP file is then exported and transferred to the operator so that integration into the Process Orchestration Layer (POL) can take place.

Phoenix Contact has already tested the MTP DESIGNER successfully with various POL providers, including ABB (System 800xA), COPA-DATA (ZENON), Siemens (SIMATICS PCS neo), and Yokogawa (CI server).

Step 1: Integration of P&IDs

The first step in MTP DESIGNER includes the transfer of the P&IDs of your systems. In the following video, our expert Oleg Makarov shows you how you can quickly and easily import data from the P&ID tool into MTP DESIGNER. This is the basis for the project work in MTP DESIGNER.

Step 2: Creating a project

MTP DESIGNER enables the integration of MTP files into the POL.
In the next step, the PLC program generated in MTP DESIGNER is transferred to PLCnext Engineer. This means that the generated file can be used on all PLCnext Controls, e.g., on an AXC F2152. The tool also generates a local visualization of the modules, enabling easy module commissioning.

The module engineering tool product range includes two libraries that describe the functions and interfaces. The “Module Type Package FB” library contains various function blocks that can be used in PLCnext Engineer. As an extension to this, the “Module Type Package HMI” library can be integrated into PLCnext Engineer and the appropriate visualization of the MTP components can be created.

Creation of an example project in MTP DESIGNER

Interactive image map: MTP DESIGNER user interface
Project structure
The project structure shows all elements used in the project. In addition, services and procedures can be created and managed within this area.
Workspace
The P&ID-mapping illustration is displayed and managed here.
Properties
Users will find further details on the objects, such as Interfaces and ECLASS. Projects can also be edited here.
Tools
All static and dynamic objects are managed here and can be inserted into the workspace from here.
Information
This window provides users with further information on how to import and export the file. Potential data traffic errors are also visible in this area.

As a system manufacturer, we need a simple and reliable tool chain that supports us from creation right through to submitting the documentation. The MTP DESIGNER enables us to realize our systems consistently and MTP-compliantly, and to program the software for the controller. We also use PLCnext Control from Phoenix Contact as a part of this process.

Michael Nussbaumer, Managing Director
Michael Nussbaumer

Advantages of the MTP DESIGNER

  • Direct integration into the POL, while the MTP module is developed in parallel
  • Configuring instead of programming – function blocks can be generated automatically from P&IDs
  • Quick and easy generation of tailored, local visualization for HMIs
Download
Test the MTP DESIGNER

Experience it for yourself and discover the versatility of the MTP engineering tool for your project.

Download the free trial version
MTP DESIGNER engineering tool

Contact


Anja Lang
Anja Lang
Vertical Market Management - Process Industry | Product Management
I would be happy to show you the advantages of using MTP DESIGNER for your project.