The content you are viewing is tailored for Global. View Content for United States | Choose Another Country

Surge protection for PV rooftop systems Find out about the ideal surge protection for your application.

People in a PV rooftop system

The challenge


Rooftop system from above

Avoid yield losses and high repair costs

In order that planned amortization times are not exceeded, long downtimes and high repair costs should be avoided. However, the effects of lightning strikes and surge voltages can cause considerable damage to the system. A surge protection concept is therefore of paramount importance for the trouble-free operation of PV rooftop systems. The concept should include the protection of the inverter, the PV panels, and, in PV rooftop systems with an external lightning protection system, the building itself.

Standards symbol

Standards requirements

Standards are an effective tool for ensuring quality, efficiency, and safety. For PV rooftop systems, the focus on two standards:

  1. HD-60364-7-712 for planning and installing PV systems
  2. EN 62305-3 Supplement 5 for the selection and installation of lightning and surge protection

What requirements must surge voltage concepts for rooftop systems meet? The following dimensioning in accordance with EN 62305-3 Supplement 5 should be of aid:

Building without external lightning protection
Building with external lightning protection – the separation distance is maintained
Building with external lightning protection – the separation distance is not maintained
Building without external lightning protection

  • Installation location DC 2 DC surge protection in the vicinity of the PV panels: type 2 surge protective devices
  • Installation location DC 1 DC surge protection in the vicinity of the inverter: type 2 surge protective devices, if the cable length between DC 1 and inverter is >10 m
  • Installation location AC 2 AC surge protection on the AC side of the inverter: type 2 surge protective devices, if the cable length between AC 1 and AC 2 is >10 m
  • Installation location AC 1 AC surge protection in the main distribution: type 2 surge protective devices

Building with external lightning protection – the separation distance is maintained

  • Installation location DC 2 DC surge protection in the vicinity of the PV panels: type 2 surge protective devices
  • Installation location DC 1 DC surge protection in the vicinity of the inverter: type 2 surge protective devices, if the cable length between DC 1 and inverter is >10 m
  • Installation location AC 2 AC surge protection on the AC side of the inverter: type 2 surge protective devices, if the cable length between AC 1 and AC 2 is >10 m
  • Installation location AC 1 AC surge protection in the main distribution: type 1 surge protective devices

Building with external lightning protection – the separation distance is not maintained

  • Installation location DC 2 DC surge protection in the vicinity of the PV panels: type 1 surge protective devices
  • Installation location DC 1 DC surge protection in the vicinity of the inverter: type 1 surge protective devices
  • Installation location AC 2 AC surge protection on the AC side of the inverter: type 1 surge protective devices
  • Installation location AC 1 AC surge protection in the main distribution: type 1 surge protective devices

The solution


String combiner box in front of a PV rooftop system

String combiner boxes for photovoltaic systems

In response to these challenges, we provide, as part of our preassembled system solutions, reliable string combiner boxes that protect the inverters in rooftop PV systems directly downstream of the DC voltage inputs. As a result, surge voltage couplings are discharged directly to the ground potential.

String combiner boxes
Product overview

Gain an overview of our product portfolio of ready-to-install and ready-to-connect string combiner boxes for your rooftop systems and find the right string combiner box for your application here.

Find the right product
Two electricians in discussion within a PV rooftop system

3 steps to your perfect string combiner box:

Electrician working
Electrician working
Electrician working
Electrician working
Electrician working

Knowing which inverter will be used is important because the following criteria are crucial when selecting the right string combiner box:

  • Number of MPP trackers
  • Number of strings per MPP tracker
  • Maximum current per MPP tracker

Electrician working

A relevant factor when selecting the right string combiner box is whether the building has or does not have external lightning protection:

Building without external lightning protection:

  • Type 2 surge protective devices are sufficient

Building with lightning protection:

  • Type 2 surge protective devices if separation distance “s” is maintained
  • Type 1 surge protective devices (or 1/2 combined lightning current and surge arresters) if separation distance “s” is not maintained

Electrician working

Choosing the right connection technology for string combiner boxes influences the efficiency, safety, durability, and ease of maintenance of the system. Two options are available here.

  • SUNCLIX connectors
  • Cable gland with Push-in Technology

More information on connection technology for photovoltaics
Electrician working

You will find the right product quickly and easily by answering the key questions above within the filter function on the product list page. The key filter criteria for narrowing down the search to the right product are therefore:

  • Number of supported MPP trackers
  • Number of strings per MPP tracker
  • Arrester class in accordance with IEC
  • Type of cable entry

If there are additional requirements (e.g., DC switch disconnector, fuses), you can also filter the search by these options. This enables you to find the right solution quickly.

Special tip: Our compatibility finder enables you to find the right string combiner box for the inverter used in just three steps.

To the string combiner boxes for photovoltaic systems

Typical structure of our string combiner boxes

Interactive image map: String combiner box configuration
Combining strings
The combination of individual strings via internal parallel connection can, for example, help to reduce the installation effort when setting up the photovoltaic system.
Combining strings
Integration of the photovoltaic system protective grounding and lightning protection equipotential bonding
Our solutions have two protective grounding connection points: one for the protective conductor of the installed surge protective device and, as an option, one for functional grounding – the lightning protection equipotential bonding of the photovoltaic system.
Integration of the photovoltaic system protective grounding and lightning protection equipotential bonding
DC surge protection
High-quality surge protective devices from Phoenix Contact protect against the effects of lightning strikes and surge voltages. They are available as type 1 and type 2 surge protective devices.
Find out more
DC surge protection
Motorized DC switch disconnector (fire department switch)
A selection of string combiner boxes is equipped with motorized DC switch disconnectors, also known as fire department switches. In the event of a fire, these switches enable DC cables in the building to be switched to a load-free stated quickly and easily. You will find a product list of all available products here.
Find out more
Motorized DC switch disconnector (fire department switch)
Manual DC switch disconnectors
Manual DC switch disconnectors enable the PV strings to be disconnected safely during maintenance and repair work. You will find a product list of all available products here.
Find out more
Manual DC switch disconnectors
PV fuses
If you need to use fuses in your application, you will find a product list with all our available products here.
Find out more
PV fuses

Your advantages

  • Protection of a wide range of inverters downstream of the DC voltage inputs with our broad product portfolio
  • Fast installation and startup with preassembled string combiner boxes
  • Simplified connection of the lightning protection potential balancing conductor with sufficient connection options in the string combiner box
  • Maintenance-free connection of PV strings with SUNCLIX or Push-in connection technology
Housefire with fire and smoke

Safe disconnection in the event of a fire

There is no general regulation for so-called fire department switch disconnectors in rooftop PV systems, but fire protection organizations and insurers are increasingly recommending their use.
The main objective is to “automatically” switch off the PV strings as close to the PV panels as possible in the event of an emergency. This minimizes the risks for the emergency services. Safe firefighting is ensured.

String combiner box with switch disconnector

Automatic shutdown with the fire department switch disconnector

Regardless of whether the building is equipped with a photovoltaic system or not, a voltage-free state must be ensured before any extinguishing work can be started in the affected area. This can be ensured, for example, by actuating the main switch or by pulling fuses. This approach also interrupts the power supply of the motorized switch disconnectors in the string combiner box, which “automatically” de-energizes the DC cables in the building. Another advantage is the motorized reactivation of the switch disconnector. Intentional, unintentional, or mains failure-related shutdowns do not lead to expensive service actions, because the switch disconnectors are reactivated via motor when reset.

Important information and frequently asked questions (FAQ)

Electricians in discussion

Discover many more exciting aids in the field of surge protection for PV systems and the use of string combiner boxes in our comprehensive FAQs section. You will find detailed answers and helpful information to help you plan and implement your projects here.

Contact


Contact

Photograph of people
Ihre Experten für Generatoranschlusskästen
Product management
We will be happy to support you in selecting the right string combiner box for your photovoltaic system.

Further products


Frequently Asked Questions


DC switch disconnectors

When does it make sense to use a DC switch disconnector?

A DC switch disconnector is mandatory in every photovoltaic system, because it contributes to safety and ease of maintenance. Connections can only be disconnected safely in a load-free state. Switch disconnectors are often integrated into the inverter; however, a large part of the system remains live when long cables are used. This should be prevented during maintenance and repair work.
The solution: installing an additional DC switch disconnector closed to the PV panels. Our string combiner boxes combine this switch with surge protection and simplify the cable installation up to the inverter.

PV fuse

Fuses: Why do they play a secondary role in rooftop systems?

In Europe, according to HD 60364 Part 7-712, PV fuses are only required in systems with three or more parallel-connected PV strings per MPP tracker. In systems with three or more PV strings connected in parallel, residual currents can damage modules and cables. In such cases, PV fuses are crucial for avoiding personal injury and damage to buildings. Many of the latest inverters only allow the connection of up to 2 strings per MPP tracker. Information on reverse current resistance and maximum fuse protection can be found in the module manufacturer’s data sheet. Among the exceptions are PV systems with DC power optimizers or inverters with selective string shutdown, which can prevent residual currents. In this case, it is sometimes possible to do without PV fuses, although it is imperative that manufacturer’s information is always observed.

PV connection technology

Which connection technologies are available?

Selecting the right connection technology for string combiner boxes has a decisive influence on the efficiency, safety, durability, and ease of maintenance of the system. Two options are available:

1. Plug-in connection technology: SUNCLIX
This technology features a high level of ease of installation and ease of maintenance. The required connectors are supplied with the string combiner box, and thanks to the spring connection technology, a crimping tool is not required. The patented unlocking mechanism works without special tools and also enables compact string combiner box designs.

2. Direct connection via connection terminal blocks with Push-in Technology
In addition to plug-in solutions, the cables can also be inserted via cable glands. Connection terminal blocks with Push-in Technology enable easy and direct conductor connection.

String combiner box

Is it also possible to connect aluminum conductors?

Aluminum conductors are a popular choice in photovoltaic installations due to their low weight and cost efficiency. However, they require special connection terminal blocks and technologies for ensuring a safe and permanent connection. Because standard SCBs are not designed for the direct connection of aluminum conductors, tailor-made solutions are required. These prevent corrosion and contact problems.

Weather protection canopy

Is it possible to use them in unprotected outdoor areas?

Installing string combiner boxes (SCBs) in unprotected outdoor areas is sometimes unavoidable. Even though SCBs with a degree of protection of IP65 are dust-proof and protected against jet water, the tests in accordance with DIN EN 60529 are only comparative and do not simulate any real conditions. Weatherproof canopies are therefore essential. They protect string combiner boxes installed outdoors from becoming waterlogged, overheated due to sunlight, and condensation. They therefore significantly increase the service life and reliability of the string combiner boxes.

String combiner box with large field connectors

How can line losses be minimized?

Due to varying location conditions, certain PV rooftop systems may need very long cables. To minimize power dissipation, it may be necessary to increase the cable cross-sections. A large number of standard SCBs can only accommodate a limited range of connection cross-sections. A selection of our versions, on the other hand, enables an extended connection cross-section to meet these requirements.

Two people in a photovoltaic rooftop system

What should be considered when installing an external lightning protection system?

A photovoltaic system and an external lightning protection system share the roof space. The PV system and lightning protection system can be installed at the same time without any problems. When retrofitting a photovoltaic system on a roof on which a lightning protection system is already installed, several aspects must be taken into consideration. Find out more about separation distances, slopes, shading, and cable routing here.

Two people in discussion in a PV rooftop system

Still haven’t found the right product?

Feel free to contact us. We will consult with you to find the ideal solution together.