Increasing the availability of conveyor belts In machine building, conveyor belts are intelligently switched and turned with CONTACTRON hybrid motor starters.

Filtration solutions from Hengst ensure that motors work cleanly and efficiently

Hybrid motor starters from Phoenix Contact are used to drive the conveyor belts in the assembly plants of Hengst SE & Co. KG. Hengst opted for the hybrid motor starters due to their robust design, simple wiring and operation, and 10-times longer service life. This increases system availability.

Filtration and fluid management production hall at Hengst SE & Co. KG

Hengst SE & Co. KG

Hengst SE & Co. KG develops and manufactures filtration solutions and filters that ensure motors work cleanly and efficiently in cars, commercial vehicles, and ships. The filter systems ensure that motors and machines work more cleanly and efficiently.
Family-owned Hengst SE & Co. KG was founded in 1958 in Münster, Germany. The company has around 3,000 employees at various international sites.

Hybrid motor starters in the control cabinet of a Hengst SE & Co. KG assembly plant

Hybrid motor starters in the assembly plant at Hengst SE & Co. KG

The products from Hengst are produced with extensive manufacturing capability. This ensures independence from external suppliers as well as the highest level of flexibility and quality. All in-house production systems, including software and electrical design, are planned, built, and installed by the company. This ensures that the systems are up to meeting the applicable requirements, demonstrate a high level of availability, and that maintenance is optimized to suit individual needs.

The quality of the components used in the system, easy operation, and the durability of the components is of great importance. With this in mind, Hengst uses CONTACTRON hybrid motor starters from the Phoenix Contact product family to operate the conveyor belts installed in its high-quality assembly plants.

The robust design and straightforward wiring and operation were our reasons for choosing CONTACTRON.

Alfons Lehmbrock - Hengst SE & Co. KG, Project engineer for in-house machine building
Photo of Alfons Lehmbrock, project engineer for in-house machine building at Hengst SE & Co. KG
CONTACTRON hybrid motor starters

Longer maintenance cycles with hybrid motor starters

The service life of CONTACTRON hybrid motor starters is ten times longer, which is also an advantage because Hengst works with high switching frequencies. This significantly extends maintenance cycles, and the availability of the system is increased. The hybrid motor starters, which are ideal for motor types with a power of up to around 3 kW, are also suited for use in small freight lifts in addition to conveyor belts.

Contact
Customer service
Phoenix Contact GmbH & Co. KG
+49 5235-300
Different CONTACTRON hybrid motor starters on DIN rails
Phoenix Contact CONTACTRON pro YouTube

Explore all of our hybrid motor starters Switching, reserving, and protecting three-phase asynchronous motors

Would you like to know how you can switch, reserve, or protect your three-phase asynchronous motors from 50 W to 3 kW? If so, contact us or take a look at our intelligent switching devices here.