The content you are viewing is tailored for Global. View Content for United States | Choose Another Country

RFID reader for AC charging controllers with LED indicator and buzzer

2024-05-20
RFID reader for AC charging controllers

The new RFID reader with configurable LED indicator and buzzer from Phoenix Contact is used in conjunction with the CHARX control modular charging controllers and is suitable for mounting in home chargers and charging stations.

The RFID reader features a bright, four-color LED status indicator as well as a buzzer for acoustic feedback during RFID interactions. This provides users of the charging stations with intuitive feedback on the RFID and charging status – the LED indicator lights up, flashes, or pulsates with adjustable brightness in four selectable colors, and the buzzer sounds at an adjustable volume.
The RFID reader can be easily configured using a web browser or configuration tool for CHARX control modular, and an NFC interface for future function extensions is also available.

Press Contact
Eva von der Weppen
Eva von der Weppen | Corporate Communications