The content you are viewing is tailored for Global. View Content for United States | Choose Another Country

Welcome to the All Electric Society Park

Tomorrow’s sustainable world, today’s technologies.
Overview of the All Electric Society Park and the flow of electrical energy

Experience, discover, and explore the future:

How reliable are renewable energy sources? Where do we get energy from when the sun is not shining and the wind is not blowing? Why are there different ways to charge an electric car? And how does the green electricity actually get into the car, a building, or production?

Our All Electric Society answers these and other exciting questions: Experience live with us in Blomberg how energy is generated, stored, and distributed and how energy consumption is optimized – and how all these areas relate to each other.

First impressions of the All Electric Society Park

The All Electric Society Park
People in front of a wind turbine nacelle in the All Electric Society Park
A woman and a man in front of a monitor in the All Electric Society Park
A man and two children at an interactive wall in the All Electric Society Park
Night shot of the All Electric Society Park with the wind tree and solar tracker

Plan your visit to us

  • Opening hours The All Electric Society Pavilion and Cubes: Monday through Sunday from 7:00 a.m. to 9:00 p.m.
  • The grounds of the All Electric Society Park are freely accessible and can be visited at any time.
  • Admission: Admission is free of charge.
  • Target group: The park is suitable for all ages. The applications are explained in such a way that children and visitors without a technical background can understand the subjects relating to the All Electric Society.
  • Address: Flachsmarktstrasse 8, 32825 Blomberg, Germany

The All Electric Society Park at a glance

Interactive image map: Map of the All Electric Society Park
Energy Storage
Our battery storage systems store surplus renewable energy. This energy is used when the sun is not shining, the wind is not blowing, or when there is a high energy demand. The battery storage systems are integrated optimally into the power supply with reliable connection and automation technology.
Phoenix Contact provides the solutions for this
Energy Storage
Power-to-X
Converting electrical energy into hydrogen enables it to be stored. The process is known as electrolysis. The stored energy can be used during periods when it is not possible to generate renewable energy. Monitoring and automating processes is crucial for reliable operation.
These solutions from Phoenix Contact facilitate this
Power-to-X
Thermodynamical Center
Thermal power distribution ensures that all buildings in the All Electric Society Park are supplied with heating and cooling. Here, we demonstrate the heating and cooling circuit and explain how we use an ice storage system for heating. Intelligent building automation ensures optimum air conditioning.
These solutions from Phoenix Contact facilitate this
Thermodynamical Center
Water and Environment
A sustainable world needs more than just renewable energy. We also have to work with all of our valuable resources responsibly. We therefore use automated and on-demand irrigation in the All Electric Society Park. We explain how this works here.
Phoenix Contact provides the solutions for this
Water and Environment
Wind Power
The All Electric Society Park includes a real wind turbine nacelle. We use this to demonstrate just what a wind turbine generator has to endure during storms and snow. The systems are monitored to ensure that electricity is generated reliably, even during bad weather. This makes it possible to respond to any weather events in good time.
Phoenix Contact provides the solutions for this
Wind Power
Solar Power
Solar power is the source of sustainable electricity in the All Electric Society Park. Solar panels are located on all roofs, on the facades of the pavilion, and even integrated in paths. For the energy transition to succeed, solar power must be fed into the power grid quickly and reliably.
These solutions from Phoenix Contact facilitate this
Solar Power
Substation
The secondary substation makes the renewable energy available to the All Electric Society Park. Two transformers ensure that the frequency and voltage are correct. In the event of a failure, we would have no more electricity. Secondary substations are monitored digitally so that any malfunctions can be detected and rectified quickly.
Phoenix Contact provides these solutions for this
Substation
Power Center
Electrical power distribution ensures that the All Electric Society Park is supplied with electricity. The challenge is to keep the power grid stable despite distributed feed-in. Here, we demonstrate that the right balance between energy generation and its use is crucial for this.
Phoenix Contact provides the solutions for this
Power Center
E-Mobility
E-mobility is an important component on the way to a sustainable future. Here, we demonstrate how the energy is fed into the electric car and how it does not always have to be used to drive the car. Powerful charging technology makes e-mobility suitable for everyday use.
Phoenix Contact provides the solutions for this
E-Mobility
The All Electric Society Pavilion
The All Electric Society Pavilion is the ideal starting point for your visit. Here, we explain our vision of the All Electric Society. Sector coupling is a key element in this. It creates an overall system comprising mobility, infrastructure, industry, and energy that only uses renewable energy.
Further information on the All Electric Society
The All Electric Society Pavilion

The All Electric Society Park is designed to enable you to develop your solution yourself. There are a host of different information sources available for this.

You will find the following on the monitors in the glass cubes and in the pavilion:

  • Overview of the All Electric Society Park with all energy and data flows and information windows in “PARK” view
  • Explanatory videos to match the topic of the cube in “CUBE” view
  • In-depth technical information provided in “EXPERTS” view

The monitors are touch-activated, so you can choose yourself what you want to see. Interactions are integrated in the glass cubes to match the relevant topic. You can use these fun elements to experiment and see for yourself what the technology does in the All Electric Society.

There are QR codes on the different objects everywhere in the park. You can scan them with your smart phone to get more information about the object.

The best place to start is to visit the All Electric Society Pavilion. You can then choose which stations to visit next.

What is the All Electric Society?

In the All Electric Society, only renewably-generated electrical energy is used. However, these sustainable actions do not automatically mean doing without. Instead, it is a matter of using existing resources optimally and making them available equally to everyone in the world.
This is made possible by sector coupling: the linking of all relevant areas of life and work – mobility, energy, infrastructure, and industry – to form one system. In this system, the energy is distributed automatically in accordance with demand. This ensures that it is always available where it is needed.

A great idea for the future, in a compact size

The All Electric Society Park lit up at night
Wind turbine nacelle in the All Electric Society Park
Overview of the visited All Electric Society Park
Tracked solar tracker in the All Electric Society Park
Control cabinet in the All Electric Society Park
The All Electric Society Park lit up at night

It is a little larger than a soccer field. As the park’s centerpiece, the All Electric Society Pavilion shows what the All Electric Society means at Phoenix Contact and how sector coupling helps optimize the flow of renewable energy.

Wind turbine nacelle in the All Electric Society Park

It is the nacelle that ensures that a wind turbine generator can be operated at lofty heights. This sensitive area is usually only accessible to specialists, but in our park you not only have the opportunity to take a close look at the powerhouse, but also go inside it.

Overview of the visited All Electric Society Park

Interactive glass cubes around the site make experiencing the All Electric Society topics a fun adventure. All cubes are intelligently networked with each other. This means that you can always tell how much energy is available and where it is needed.

Tracked solar tracker in the All Electric Society Park

Around 550 solar panels in the All Electric Society Park ensure that it can be fully supplied with renewable energy. In addition to roof panels and solar panels integrated into windows, there are 26 m² of walkable solar paving integrated in the paths.

Control cabinet in the All Electric Society Park

Connect everything together in the All Electric Society Park. Here, electricity flows through cables that have a total length of 7 km. The other 12 km of cables are needed for data connections.

The All Electric Society Park – the making-of

FAQs

Dice with question mark
Dice with question mark
Parking spaces with charging stations for electric cars at the All Electric Society Park
Dice with question mark
Dice with question mark
Dice with question mark

Yes. Access is also possible for wheelchairs, strollers, etc.

Dice with question mark

No. In the All Electric Society Park, the basics for a sustainable and livable world are explained in such a way that even people without a technical background can understand the technical solutions.

Parking spaces with charging stations for electric cars at the All Electric Society Park

Yes, there are three type 2 AC charging stations with 22 kW (32 A/400 V) that can be used for a fee. At these charging stations, there is the option of price-variable charging via a Giro Card and charging via negotiated roaming tariffs.

Dice with question mark

You should allow 60 to 90 minutes for your visit so you can see everything at your leisure. Of course, this varies depending on how much each subject interests you.

Dice with question mark

The washrooms are located in the basement of the All Electric Society Pavilion. Access is via the external staircase at the side of the building.

Wheelchair users should ring the bell at the door to the staircase on the first floor of the pavilion. We will then show you the way to the elevator.