Click-in module carrier frames for heavy-duty connectors

2025-10-01
Heavycon module carrier frames with click-in latching

The new Heavycon series click-in module carrier frame from Phoenix Contact simplifies the assembly and installation of heavy-duty connectors significantly. The tool-free click-in latching system enables the inserts to be mounted quickly and reliably – without any screws.

An audible and tactile click signals the correct position and ensures maximum process reliability while reducing time expenditure to a minimum. The protective conductor can be connected easily and without tools using the proven Push-in Technology for the protective conductor contact. A special feature is that the protective conductor contact can also be fitted when installed. This facilitates installation in confined spaces and increases efficiency.

The compact multi-medium connectors transmits power, signals and data simultaneously and saves space in the control cabinet with their individual configurability. Power modules specially designed for high currents enable reliable transmission of up to 300 A. This makes them ideal for power-intensive applications such as energy storage systems and server racks.

Press Contact
Eva von der Weppen
Eva von der Weppen | Corporate Communications & Brand Management