Identifying and eliminating efficiency gremlins in control cabinet building

Small causes, big impact: Many small efficiency gremlins often slow down productivity without anyone noticing, and they add up to significant losses. It is time to bring them to light and eliminate them systematically.
Workbench with terminal blocks, hand tools, and conductors
Efficiency gremlins depicted as small, green, fluffy monsters

Have efficiency gremlins long since become the norm in your everyday life, too?

Monday morning in control cabinet building. The order seems clear enough, and yet the process grinds to a halt because tools are missing, materials are not on hand, and the information doesn’t add up. Instead of clear processes, there are delays, coordination work is necessary, and improvised solutions are created.

These are just minor interruptions that no one really questions. But that is precisely the problem. After all, although individual issues may go unnoticed, they add up over the course of the day, the order, and the entire production process: time spent searching, making unnecessary trips, duplicating steps, and unclear information put the brakes on value creation. We call these silent losses efficiency gremlins. The tricky thing is that most of the efficiency gremlins are invisible and have long since become part of daily activities. But anyone who can identify them can address them – often with just small targeted changes and appropriate solutions.

Typical efficiency gremlins in control cabinet building


Materials on a workbench in control cabinet building

When trips cost time Efficiency gremlins surrounded by walking distances, reach distances, and time spent searching for materials

The component is not where it should be, and the tool needed is missing or is at the other end of the workshop. This means walking, handling, and searching. And not just once a day. A total of 82% of companies carry out workshop assembly work. At the same time, 64% of control cabinet builders do not use lean methods. The consequences overall include excessively long search times, unnecessary trips, interrupted workflows, and a lack of focus on the actual work. What seems to take just a few seconds slowly adds up over the course of the day to real losses in efficiency due to many small, avoidable trips and unstructured material provision.

A torn circuit diagram amongst paper documentation

When information slows things down Efficiency gremlins surrounded by paper, data chaos, and media discontinuities

Missing data, outdated information, manual data maintenance, and hardcopy documentation: Instead of working, employees spend their time searching, cross-checking, and asking for clarification. An incredible 88% of control cabinet builders still use paper in their manufacturing processes; just 12% operate entirely digitally. At the same time, 88% of companies receive customer data in PDF format, with real engineering data being the exception. This results in media discontinuities, duplicate upkeep work, version chaos, and wasted time due to missing, unclear, and scattered information.

A worker stripping insulation from a wire

When manual steps become a source of error Efficiency gremlins: laborious work, subprocesses, and loss of precision

In control cabinet building, manual tasks ranging from assembling components on DIN rails, through conductor assembly, right through to wiring are a feature of the daily routine. A total of 86% of German control cabinet builders operate with a low level of automation, and just 14% use assistance systems. What appear to be routine tasks add up to significant time losses in the daily workflow. At the same time, repetitive tasks lead to an increased likelihood of errors and inconsistent quality. A large number of discrepancies go unnoticed, but they often lead to time-consuming and costly rework.

Do not delay. Make an appointment now.
It is time to get even!

Have you identified efficiency gremlins, or do you want to put your production process to the test? With our experience and an outside perspective, we bring hidden potential to light. Don't let things annoy you any longer. Reclaim your lost value creation.

Arrange a consultancy appointment
A Phoenix Contact consultant explaining a value stream analysis using a flip chart

Your personal contact person

Working together to combat efficiency gremlins in control cabinet building

Jafar Parakkanni
Jafar Parakkanni
Product Manager
Have you identified efficiency gremlins, or do you want to put your production process to the test? I will be happy to offer advice.

Our solutions for combatting efficiency gremlins

Many efficiency gremlins can be eliminated more quickly than you might think. With clear structures, well-considered workstations, and the right flow of information. This product selection highlights specific ways to eliminate efficiency gremlins in practice.

Workstations that frustrate efficiency gremlins Structured, ergonomic, efficient

Interactive Image Map: Software-supported workstation for wire preparation and wiring in a control cabinet building environment
Automatic tools instead of time-consuming piecework
The manual steps involved in cutting, stripping, and crimping can quickly become major efficiency gremlins in conductor assembly processes. Automatic tools enable the partial automation of these processes and ensure shorter production times, reproducible results, and increased process reliability.
Find out more
Automatic tools instead of time-consuming piecework
Mobile workstations instead of unnecessary trips
Mobile workstations bring materials and tools directly to where they are needed. This reduces unnecessary trips and time spent searching, lightens the load on manual processes, and ensures a more consistent workflow. An important contribution to noticeably reducing efficiency gremlins in control cabinet building.
Find out more
Mobile workstations instead of unnecessary trips
Smooth operations instead of interruptions
The conductors slip back, so you have to keep finding the end all over again. These unnecessary actions take time, interrupt the workflow, and increase the likelihood of errors. The wire brake solves this problem. It holds the conductor securely in place and prevents it from slipping back.
Find out more
Smooth operations instead of interruptions
Organization instead of long search times
Whether disorganized tool storage, time-consuming searches, or unnecessary trips – without proper organization, workflows are constantly interrupted. Workstations with drawers combined with shadow boards keep things organized: Each tool has its own designated, visually marked spot, and is immediately within reach.
Find out more
Organization instead of long search times
Data consistency instead of media discontinuities
If data is maintained in duplicate or transferred manually, the risk of errors and the amount of work involved increase. Software solutions with intelligent interfaces seamlessly link planning and production, ensuring that all data is automatically transferred and used consistently.
Find out more
Data consistency instead of media discontinuities
Automated marking instead of manual work
Many manual tasks can be time-consuming in day-to-day work and lead to errors and inconsistent quality. Printing systems for automated identification bundle work steps together: markers are printed and applied automatically – more quickly, more precisely, and with consistent quality.
Find out more
Automated marking instead of manual work

Working together to combat efficiency gremlins


Process consulting in control cabinet building

Process consulting in control cabinet building

In everyday life, efficiency gremlins creep in everywhere and often become a habit. Even though they may seem small at first glance, they add up to significant losses. This is exactly where our process consulting comes in. Together, we will identify both the obvious and hidden inefficiencies at your workplace. We don't just look at individual work steps, but at the interplay between employees, materials, and information. Building on this, we work with you to develop customized solutions that are tailored to your production needs. The key point here is that even small changes can lead to significant efficiency gains. And this is why we optimize your processes step by step – working together, with a practical approach, and in a way that can be implemented immediately.