Drivers

Axiobus
Axiobus

Axiobus is the built in IO communication system of Phoenix Contact AXC F controllers and devices. The axiobus driver supports Axiobus IO modules and Smart Elements IO devices.

On initial bootup, the Axiobus driver will be running, and the status should be "OK".

Axiobus driver

Clicking on the Axiobus dashboard item will take the user to the Axiobus status page where the user can view more detailed Axiobus information.

Axiobus status page

On the Axiobus page, the interface displays the current Axiobus installation. At the top, a graphical bus representation validates that the modules installed are being accessed by the PLCnext Edge Gateway. At the top right, clicking the gear icon will take the user to the bus settings page where modules can be configured and bus configuration saved. On the left navigation bar, the logs tab presents logs produced by the Axiobus driver for diagnostic purposes.

In the lower section, each attached module provides status and meta data ("Order"/Part Number and Serial Number) for each installed module. By clicking on the desired module in the module list, the active IO values are displayed.

Axiobus installation