Welcome to the All Electric Society Park

Tomorrow’s sustainable world, today’s technologies
All Electric Society Park by Phoenix Contact

Experience, discover, and explore the future:

How reliable are renewable energy sources? Where do we get energy from when the sun is not shining and the wind is not blowing? Why are there different ways to charge an electric car? And how does the green electricity actually get into the car, a building, or production?

Our All Electric Society answers these and other exciting questions: Experience live with us in Blomberg how energy is generated, stored, and distributed and how energy consumption is optimized – and how all these areas relate to each other.

First impressions of the All Electric Society Park

All Electric Society Park, Blomberg, aerial photograph
Wind tree in the All Electric Society Park
Solar tracker at the All Electric Society Park
Wind turbine nacelle in the All Electric Society Park
The All Electric Society Park

Plan your visit to us

  • Opening hours The All Electric Society Pavilion and Cubes: Monday through Sunday from 7:00 a.m. to 9:00 p.m.
  • The grounds of the All Electric Society Park are freely accessible and can be visited at any time.
  • Admission: Admission is free of charge.
  • Target group: The park is suitable for all ages. The applications are explained in such a way that children and visitors without a technical background can understand the subjects relating to the All Electric Society.
  • Address: Flachsmarktstrasse 8, 32825 Blomberg, Germany

The interactive park experience

Interactive image map: The All Electric Society Park, Blomberg
Energy storage
Our battery storage systems store excess renewable energy. This energy is used when the sun is not shining, when the wind is not blowing, and when the high energy consumption is high. The battery storage systems are integrated optimally into the power supply with reliable connection and automation technology.
Phoenix Contact provides the solutions for this
Energy storage
Power-to-X
This energy can be stored by converting electrical energy into hydrogen. The process is known as electrolysis. The stored energy can be used during times when it is not possible to generate renewable energy. Monitoring and automating processes are crucial for reliable operation.
These solutions from Phoenix Contact facilitate this
Power-to-X
Thermodynamics center
The thermal power distribution system ensures that all buildings in the All Electric Society Park are supplied with heating and cooling. Here, we demonstrate the heating and cooling circuit and explain how we use an ice storage tank for heating. Intelligent building automation ensures optimum air conditioning.
These solutions from Phoenix Contact facilitate this
Thermodynamics center
Water and environment
A sustainable world needs more than just renewable energy. We also have to work with all of our valuable resources responsibly. To this end, we use automated and needs-based irrigation in the All Electric Society Park. We explain how this works here.
Phoenix Contact provides the solutions for this
Water and environment
Wind power
The All Electric Society Park includes a real wind turbine nacelle. We use this to demonstrate just what a wind turbine generator has to endure during storms and snow. The systems are monitored to ensure that energy is generated reliably, even during bad weather. These monitoring systems make it possible to respond to any weather events in good time.
Phoenix Contact provides the solutions for this
Wind power
Solar power
Solar power is the source of sustainable electricity in the All Electric Society Park. Solar panels are located on all roofs, on the facades of the pavilion, and even in the sidewalk. Solar power must be fed into the grid quickly and reliably if we are to succeed in the energy revolution.
These solutions from Phoenix Contact facilitate this
Solar power
Substation
The secondary substation makes the renewable energy available to the All Electric Society Park. Two transformers ensure that the frequency and voltage are correct. In the event of a failure, we would no longer have any energy. Secondary substations are monitored digitally so that any malfunctions can be detected and rectified quickly.
Phoenix Contact provides these solutions for this
Substation
Power center
The electrical power distribution system ensures that the All Electric Society Park is supplied with power. The challenge is to keep the grid stable despite the decentral feed-in. Here, we demonstrate that the right balance between energy generation and its use is crucial for this.
Phoenix Contact provides the solutions for this
Power center
E-mobility
E-mobility is an important component on the way to a sustainable future. Here, we demonstrate how the energy is fed into the electric car and how it does not always have to be used to drive the car. A powerful charging technology makes e-mobility suitable for everyday use.
Phoenix Contact provides the solutions for this
E-mobility
The All Electric Society Pavilion
The All Electric Society Pavilion is the ideal starting point for your visit. Here, we explain our vision of the All Electric Society. Sector coupling is a key element in this. It creates an overall system of mobility, infrastructure, industry, and energy that only uses renewable energy.
Further information about the All Electric Society
The All Electric Society Pavilion

In our All Electric Society Park, we will introduce you to interactive stations that showcase the many ways renewable energy can be generated, converted, stored, distributed, and used. To do this, we use both self-generated green electricity and heat energy from heat pumps and conversion processes.

The All Electric Society Park is designed to enable you to develop your solution yourself. There is a host of different information sources available for this.

You can find the following on the monitors in the glass cubes and in the pavilion:

  • Overview of the All Electric Society Park with all energy and data flows and information windows in “PARK” view.
  • Explanatory videos to match the topic of the cube in “CUBE” view.
  • “EXPERTS” view provides more detailed technical information.

The monitors are touch-activated, so you can choose yourself what you want to see.
Interactions are integrated in the glass cubes to match the relevant topic. Use these playful elements to experiment and see for yourself what the technology does in the All Electric Society.

There are QR codes on the different objects everywhere in the park. Use your smart phone to scan them and obtain even more information about the object.

The best place to start is to visit the All Electric Society Pavilion. You can select the next stations as you see fit.

What is the All Electric Society?

In the All Electric Society, only renewably-generated electrical energy is used. However, these sustainable actions do not automatically mean doing without. Instead, it is a matter of using existing resources optimally and making them available equally to everyone in the world.
This is made possible by sector coupling: the linking of all relevant areas of life and work – mobility, energy, infrastructure, and industry – to form one system. In this system, the energy is distributed automatically in accordance with demand. This ensures that it is always available where it is needed.

A great idea for the future, in a compact size

The All Electric Society Pavilion
Walk-in wind turbine nacelle in the AES Park
The AES Park from above
AES Park, Blomberg, solar tracker
AES Park components
The All Electric Society Pavilion

It is a little larger than a soccer field. As the park’s centerpiece, the All Electric Society Pavilion shows what the All Electric Society means at Phoenix Contact and how sector coupling helps optimize the flow of renewable energy.

Walk-in wind turbine nacelle in the AES Park

It ensures that a wind turbine generator is operated at a lofty height: the wind turbine nacelle. Usually this sensitive area is accessible only for specialists, but in our park you not only have the chance to get a close look at the machine room. You can also to enter it.

The AES Park from above

Interactive glass cubes around the site make experiencing the All Electric Society topics an enjoyable adventure. All cubes are intelligently networked with each other. This means that you can always tell how much energy is available and where it is needed.

AES Park, Blomberg, solar tracker

Around 550 solar panels throughout the All Electric Society Park provide it with a complete supply of renewable energy. In addition to roof panels and solar panels integrated into windows, there are 26 m² of walkable solar paving integrated into the sidewalks.

AES Park components

Connect everything together in the All Electric Society Park. Here, electricity flows through cables that have a total length of 7 km. The other 12 km of cables are needed for data connections.

Why you should not miss the All Electric Society Park.

  • Because real applications let you experience how we will create the energy revolution together
  • Because you can discover what is already technically feasible today and what diverse opportunities there are in the industry to become more sustainable
  • Because you can learn hands-on and discover: Interactive elements let you become part of the energy flow
  • Because in our All Electric Society Park, you meet people who are helping to shape the future – and you can always experience something!

The All Electric Society Park – the making-of

FAQs

Dice with question mark
Dice with question mark
Parking spaces with charging stations for e-car at the All Electric Society Park
Parking spaces with charging stations for e-car at the All Electric Society Park
Dice with question mark
Dice with question mark
Dice with question mark

Yes. Access is also possible for wheelchairs, strollers, etc.

Dice with question mark

No. In the All Electric Society Park, the basics for a sustainable and livable world are explained in such a way that even people without a technical background can understand the technical solutions.

Parking spaces with charging stations for e-car at the All Electric Society Park

You can get there by car or bicycle via Schieder-Schwalenberg and Blomberg. There are plenty of parking spaces for cars and bicycles on site. Bus stops for regular bus services are right next to the All Electric Society Park. The 732 bus line runs here. The nearest train stations are Schieder-Schwalenberg and Bad Pyrmont. Buses for large groups should report to the Phoenix Contact reception desk to find out about parking arrangements.

Download parking facilities map
Parking spaces with charging stations for e-car at the All Electric Society Park

Yes, there are two fee-based type 2 AC charging stations with a power of 22 kW (32 A / 400 V) available. At these charging stations, there is the option of price-variable charging via a Giro Card and charging via negotiated roaming tariffs.

Dice with question mark

You should allow 60 to 90 minutes for your visit so you can see everything at your leisure. Of course, this varies depending on how much each subject interests you.

Dice with question mark

The washrooms are located in the basement of the All Electric Society Pavilion. These are also accessible with wheelchairs.