Sustainability project

China creates connections for increased sustainability

“AES Youth” shapes values for the common good.
Chinese Phoenix Contact employee at an event on Youth Day

Project goal

With the “AES Youth Freecycle”, the Chinese subsidiary has launched an event with the aim of sharing unused items with others. The highlights in May were the so-called blind boxes and interactive discussions.

Milestones

  • Creating awareness of unused items from everyday life
  • Event on Youth Day (May 4)

1,000

participating young people

Chinese Phoenix Contact employees at the AES Youth Freecycle

Strengthening interpersonal and material values

Passing on love and sustainability: Phoenix Contact China launched the first “AES Youth Freecycle” event for the common good on Youth Day on May 4. Here, unused items were passed on to new owners.

As their standard of living improves, many people accumulate possessions over the years which, if left unused, lead to a considerable waste of resources. To give these items new value, Phoenix Contact China urges people to donate these unused items. They are then passed on to new owners via the blind box concept.

Chinese Phoenix Contact employees at the AES Youth Freecycle

Creating connections that go beyond the shared objects

Low entry barriers and a high level of participation: More than 1,000 people took part in the campaign in May. Items such as children’s toys, household goods, books, publications, and arts and crafts have set off on new adventures. At zero cost, without emissions, and with sustainability. In addition to the value of the items, donors and recipients had the opportunity to create a personal connection. The discussions about the donated items, the surprise effect when opening the blind boxes, and ultimately the will to do good led to a great multiplier effect. A connection between individuals, the community, and even the planet.

All “AES Youth” participants continue to spread the power of sustainability, translating good will into concrete actions and making sustainability visible. A continuation of the event is already being planned.

Image for sustainability development goal number 12
Responsible consumption and production

Sustainable handling of objects

So cool to be an “AES Youth”! Behind the exchange of unused items lies not only the surprise of opening blind boxes, but also the visualization of sustainability.

Qian Xiujuan - Phoenix Contact China, MarCom and DXM Manager

Connect with us

Qian Xiujuan
Qian Xiujuan
MarCom and DXM Manager

This might also interest you