The content you are viewing is tailored for United Arab Emirates. View Content for United States | Choose Another Country

IO-Link

IO-Link is the first internationally standardized I/O technology for communicating with sensors and actuators.
Communication via IO-Link
IO-Link logo

What is IO-Link?

IO-Link is the first globally standardized I/O interface. The technology has established itself as the communication standard in machine building and systems manufacturing. The number of products with IO-Link interface used is growing rapidly. The communication standard offers you many advantages, creates new application opportunities, and constitutes an investment in important matters such as the Industrial Internet of Things (IIoT). By definition, IO-Link is an open, serial point-to-point communication protocol for connecting sensors and actuators to an automation system.

IO-Link Safety implements safe communication from start to finish. This means that users also benefit from typical IO-Link advantages in the field of functional safety, such as simple parameterization with IODD or fast device replacement.

Advantages of IO-Link

  • Increased productivity
  • Simplified installation, maintenance, and replacement processes
  • Increased data availability and accuracy
  • Troubleshooting via remote diagnostics
Signal light in production

Productivity

IO-Link devices provide the controller with detailed condition data. This data aids maintenance planning because you can identify problems quickly. If you as a user receive a warning message from dirty sensors every six months, for example, you can plan cleaning them twice a year at convenient times. Furthermore, real-time fault detection of devices enables you to reduce operating costs by minimizing unplanned downtimes.

Installation in the control cabinet

Simplicity

Everything in IO-Link is easy. Installation is easy because you can use standard cables and connectors. Maintenance is easy because you can monitor your systems and modify the settings. Using the error detection feature of IO-Link devices, you can determine the cause of a problem quickly and easily. The replacement process is also easy because the parameter data is stored in the controller. If an IO-Link device needs to be replaced, the stored parameters are automatically copied to the IO-Link device without using a programming device. As a result, your system is quickly ready to operate again.

Data analysis on screen

Increased data availability and accuracy

Analog sensors without IO-Link often pass through multiple A/D conversions before data reaches the controller, which may result in errors. In IO-Link devices, there is only one A/D conversion. This increases measuring accuracy and thus the accuracy of the entire process.

Remote configuration on a PC

Remote configuration

You can modify the parameters of the IO-Link device from your desk by responding to status messages. You therefore no longer have to shut down the production line and physically access the devices in order to rectify faults.

Components of an IO-Link system

The architecture of an IO-Link system consists of a controller, an IO-Link master, and one or more IO-Link devices. They are connected by simple three-wire, unshielded cables, which makes installation easier and more cost-effective.

Interactive image map: Components of an IO-Link system
IO-Link master
The master provides the interface to the higher-level controller, controls communication with the connected IO-Link devices, and stores parameter data and the IODD (IO Device Description) file. This file contains a device description and parameter information regarding the IO-Link device, including the manufacturer, item number, function, etc.
PLC (programmable logic controller)
The controller is used to monitor the state of the inputs and control the state of the outputs. A safety controller is required in order to process safety data.
IO-Link devices
This term refers to all intelligent sensors or actuators connected to the system such as I/Os, converters, safety relays, motor starters, or device circuit breakers. With regard to IO-Link, “intelligent” means that a device has identification data, e.g., a type designation, serial number, or parameter data. This data can be read via the IO-Link protocol. In addition, the IO-Link device can supply detailed diagnostic data that can be used for preventive maintenance and servicing.
Actuator
An actuator is an output device that converts electric signals and current into mechanical movement and thus controls mechanical installations.
Sensor
A sensor is a device that measures a physical variable (e.g., temperature, pressure, or position) and records and displays the values or provides feedback.
IO-Link Safety master
In addition to performing the tasks of a classic IO-Link master, the IO-Link Safety master enables safe communication in the field of functional safety. In addition to classic standard IO-Link devices, safety-related IO-Link devices can be connected here, such as safety sensors, safe sensors via OSSDs, safe actuators, or even mixed safety devices (e.g., mechatronic devices).
IO-Link Safety
The new standard: Secure communication from start to finish. IO-Link is an open, serial point-to-point communication protocol for connecting sensors and actuators to an automation system.
More about IO-Link Safety

What can an IO-Link device do that a standard sensor cannot?

IO-Link devices supply three types of data:

  • Process data: Condition information that the IO-Link device reads and sends to the IO-Link master or information that the IO-Link master sends to the IO-Link device. Status information is also transmitted in this process. You can thus check whether the process data is valid. An example of process data is the distance measured by a distance sensor.

  • Service data: Information that can be written to the IO-Link device or read from the IO-Link device. Example: The model or manufacturer number of the sensor helps to identify a device or configure a new one.

  • Event data: Notifications such as error messages, which are sent from the IO-Link device to the IO-Link master as soon as an event e.g., overheating, occurs.

IO-Link products

Our product portfolio for communication from start to finish: