Energy-efficient building control in the Köterhof building Modern building automation reduces the energy requirements of the historic Köterhof building in Oldenburg while creating a pleasant working environment. Innovative technology for greater efficiency and sustainability.

The Köterhof building

Customer profile


Customer meeting regarding room automation with CapitalReal GmbH & Co. KG

CapitalReal GmbH & Co. KG

CapitalReal GmbH & Co. KG specializes in the implementation of real estate and construction projects in the city of Oldenburg and the entire Weser-Ems region. The company plans, builds, sells, and rents high-quality single-family, duplex, and town houses as well as condominiums and vacation properties.

The challenge


Finn Sundermann, CapitalReal

Optimization of heating and cooling

Sophisticated design and innovative technology come together in the modern extension housing the offices of CapitalReal. Floor-to-ceiling windows with automatic shading and stylish furnishings create a pleasant working atmosphere. However, the ability to control the room air conditioning on a more individual basis was lacking, which affected the comfort of employees. In addition, the large-format room operating panels looked out of place in the high-end surroundings. EPM GmbH from Lindern was commissioned to modernize and automate the heating and cooling systems, while maintaining the original architecture and cabling infrastructure.

Solution


Catan C1 EN controller with removable display
Specialist personnel showing the I/O devices installed in the false ceiling
Catan C1 EN controller in the subdistribution
Programming, visualization, and evaluation of the Köterhof building automation system
Catan C1 EN controller with removable display

The KNX-based operating panels allow employees to heat and cool the rooms in accordance with their personal requirements. This creates a pleasant working environment and promotes both satisfaction and productivity. At night, the temperature throughout the building is lowered and, in the morning, it is ramped up to a standard value. Employees can then adjust the temperature in their room individually.

Specialist personnel showing the I/O devices installed in the false ceiling

The circulation units for heating and cooling are installed in the false ceiling. Temperature sensors and I/O devices forward the recorded values to the building controller, making efficient use of the existing infrastructure without having to lay new cables.

Catan C1 EN controller in the subdistribution

For the Köterhof project, CapitalReal relies on the compact Catan C1 EN controller. It is ideal for space-saving distribution boards and offers a wide range of communication interfaces, including Ethernet, USB-C, RS-485, and KNX TP. With 14 freely configurable I/O channels, it enables the flexible integration of functions such as temperature control, fan control, and diagnostic management. Supplemented by extension modules and a DIN rail-mounted power supply, the controller can be individually adapted for each floor.

Programming, visualization, and evaluation of the Köterhof building automation system

The Emalytics building management system offers web-based, floor-by-floor visualization and centralized control of all functions. Thanks to separate IT and OT networks, a particularly high level of cybersecurity is ensured.
In conjunction with the Niagara Framework®, Emalytics enables flexible programming and needs-based evaluation and processing of all building data – from energy monitoring to temperature control. Values can be conveniently accessed and controlled via smartphone.

Bernhard Tillmanns, Director Global Industry Management Building Technologies
Bernhard Tillmanns
Director Global Industry Management Building Technologies
I will be happy to consult with you on your modernization or new construction projects. Benefit from our long-standing experience and extensive range of services.

Products


Summary


Customer meeting regarding room automation with the Catan C1 EN building controller

Efficient retrofitting – increased comfort in young buildings

The Köterhof project shows how existing buildings can be operated efficiently and sustainably using modern automation technology. The new Catan C1 EN building controller reduces energy requirements and provides a pleasant working environment. In operation since fall 2024, various adjustments have already been made. Comparative energy efficiency figures will be available from 2026.