Grupo Jorge has been active in the meat processing industry for 75 years and is committed to adopting a sustainable approach to the available resources.
The Zuera II solar park it operates, which was connected to the grid in October 2012 with 11.5 megawatts, covers an area of more than 30 hectares and generates solar power for more than 10,000 residents.
The Zuera II solar park consists of 54,000 crystalline modules, which track the path of the sun along a single horizontal axis.
The solar park topology is divided into nine segments. Each segment is made up of 256 strings, which are connected to two central inverters via 16 string combiner boxes (SCBs). Between the SCB and the inverter station, DC meters measure the current and voltage of the DC lines. On the AC side, the converted current and voltage are determined before being fed into the power grid.
An important requirement for operators is the continuous monitoring of the strings, which ensures the stable and efficient operation of the entire system.
With this in mind, Phoenix Contact has developed a string combiner box for 16 strings, which houses the string monitoring modules from the SOLARCHECK product range as well as the necessary surge protection components.
The solar cables are connected to each SCB via external SUNCLIX plug-in connections. Potential collective terminal blocks enable the fast and space-saving interconnection of the individual strings. The SOLARCHECK measuring modules monitor the string currents and voltages. Surge protection components for DC and data cables round off the SCB solution.
An Inline small-scale controller collects the string data from the SOLARCHECK communication modules on the devices in the park. Tracking units, SOLARCHECK communication modules, DC meters, inverters, and AC meters are addressed in this way. The controller also records the temperature of the PV panels as well as the radiation values recorded via analog input terminals, and then further processes the data.
Two meteorological stations record relevant weather data, which is forwarded to a controller. This sends the data directly to the SCADA system and to the higher-level park controller via the PROFINET protocol.
Display the recorded values at any time
Operators use the web-based AXweb+ management system from Phoenix Contact, which displays performance and weather data for the solar park, for visualization and system monitoring. Operators can call the latest data via a website on which park performance is visualized either locally or via the Internet in order to gain an overview of relevant information at any time.
An error report documents failures and visualizes problems with the communication between the individual devices in the park. Maintenance personnel can access detailed information at any time at the click of a mouse.In the event of an error, the cause can be localized quickly and measures can be introduced immediately. Service employees are also notified of faults by SMS.
The complete regulation of the Zuera II solar park on the basis of string monitoring and the visualization of the recorded values secures Grupo Jorge's long-term energy yields. The group of companies chose Phoenix Contact on account of the high quality of the overall solution as well as the comprehensive support for components and systems. The automation specialist's team provided support throughout the startup phase. As all questions from the companies involved in the construction project were answered swiftly, the solar park could be connected to the grid in no time at all.
Description | Type | Order No. |
---|---|---|
String combiner box for 32 strings with Inline fuse | SOL-SC1-32-0-FI-VMC-T1-SD1-22 | 2403683 |
String combiner box for 16 strings with standard string fuse | SOL-SC1-16-0-F-VM-T1-SD1-11 | 2403682 |
Photovoltaic connector | PV-CF-S 6-16 (+) | 1790784 |
Photovoltaic connector | PV-CM-S 6-16 (-) | 1790797 |
Feed-through terminal block with spring-cage connection | STU 35/ 4X10 | 3033126 |
SCK measuring module for monitoring photovoltaic systems | SCK-M-I-8S-20A | 2903241 |
SCK communication module for data acquisition of up to 8 x SCK measuring modules | SCK-C-MODBUS | 2901674 |
Inline controller | ILC 171 ETH 2TX | 2700975 |
Inline controller with PROFINET interface | ILC 350 PN | 2876928 |
Ethernet Lean Managed Switch | FL SWITCH LM 4TX/2FX | 2832658 |
Primary-switched TRIO POWER power supply for DIN rail mounting | TRIO-PS/1AC/24DC/10 | 2866323 |
Inline digital input terminal, complete with accessories | IB IL 24 DI 16-PAC | 2861250 |
Inline RS-485/422 function terminal for serial data transmission | IB IL RS 485/422-PRO-PAC | 2863627 |
This website uses cookies, by continuing to browse, you agree to our cookie policy. Read our privacy policy for more information.
Close
"$pageName" on