FAME 3 – test plugs with patented rotary handle – the functions at a glance:
Test plug with rotary handle and locking
FAME 3 test plug with patented rotary handle
Defined, mechanically supported removal of the patented test plug from the test block. Optical display and forced locking in the various switch positions.
Step 1
Test plug inserted and locked
The test plug is inserted fully and engages securely. The display window turns red. All test contacts are contacted according to the test setup.
Step 2
Through-connected test contacts
The rotary handle is turned upward as far as it will go. The display window turns yellow. The test contacts are once again through-connected to the protective device.
Step 3
Removing the test plug
The rotary handle must be turned back to its starting position. The display window turns green. Now the mechanism releases the plug so it can be fully removed.
"$pageName" on