The content you are viewing is tailored for United Arab Emirates. View Content for United States | Choose Another Country

Valve monitoring Easily transmit valve position information to your control system wirelessly and in real time.

Manual valves in a process industry plant

The challenge


Person actuating a valve in a process industry plant

Monitoring manual valves

Manual valves come in high numbers in process plants. They meter and control liquids, air, or gases. Depending on the production step, manual valves have to be set to the correct position by plant personnel, especially in existing installations. Using checklists, employees go round the expansive plants and prepare for the startup, flushing, or cleaning of the production plant. Incorrect operation can result in production stoppages or major accidents. The open/close position of manual valves can be monitored easily to prevent such incorrect operation.

The solution


Collect data from the Ex area using the intrinsically safe I/O system

The example architecture shows a valve monitoring system based on decentral substations for acquiring the signals in zone 0 or 1. The structure of a local substation (server station) consists of the power supply, the wireless module, and the intrinsically safe input modules. The number of I/O modules is defined by the application. The system is modular. Extension via the local bus is possible.

Interactive image map: Valve monitoring system based on distributed substations
Wireless I/O communication
Radioline is the wireless system for extensive systems. It ensures that abnormal readings are immediately displayed in the operator control room so that countermeasures can be initiated at an early stage.
More about the Radioline wireless system
Wireless I/O communication
Power supplies for MCR technology
With their modular electronics housing, the MINI POWER power supplies are ideal for special voltages in measurement and control technology.
More about power supplies for MCR technology
Power supplies for MCR technology
I/O systems
For IP20 and IP65/IP67 degrees of protection
More about I/O systems
I/O systems
Valve in a processing plant

Improved intervention options

Retrofitting NAMUR limit switches and the transmission of I/O information to the control system make it possible to use software interlocks. Benefit from our preassembled control box. This gives you a continuous overview of the valve positions in the control room and, at the same time, optimum sensor diagnostics, including the cabling.

Extend the solution with various types of signals. These include, for example, temperatures, pressure values, and flow rates.

Contact

Contact person Wilfried Grote
Wilfried Grote
Director Global Industry Management Process Industry - Chemicals and Pharmaceuticals
I will be happy to advise you on scalable solutions for all aspects of comprehensive valve monitoring.

Products


Person using a tablet in front of a control cabinet

Still haven’t found the right product?

Feel free to contact us. We will consult with you to find the ideal solution together.