The content you are viewing is tailored for United Arab Emirates. View Content for United States | Choose Another Country

Compact and universal signal distribution

2023-11-14
Knife-disconnect terminal blocks with two disconnect zones

The new PT 2,5-2MTB Push-in terminal blocks from Phoenix Contact have two disconnect zones. In conjunction with the three double function shafts, they enable a wide range of distribution applications to be realized in a small space. Compared to a standard disconnect terminal block, the compact PT 2,5-2MTB reduces the length of the terminal strip by half.

The new knife-disconnect terminal block is primarily used in wind turbines, in switchgear building, in process engineering, and in machine building for complex signaling tasks. It currently serves the cross-section range from 0.14 to 4.0 mm². The disconnect zones enable multiple bridging and testing tasks to be performed in one terminal block. In addition, each terminal block has its own test pick-off. The colored disconnect knives and actuating push buttons provide a good overview.

The PT 2,5-2TGB disconnect terminal block is also available to match the knife-disconnect terminal block for use with plug-in fuse and device plugs. This terminal block also has two disconnect zones.

Press Contact
Eva von der Weppen
Eva von der Weppen | Corporate Communications