The content you are viewing is tailored for United Arab Emirates. View Content for United States | Choose Another Country

Automated identification of entire terminal strips in a single process step

2024-04-22
Thermal transfer roll printer with THERMOMARK E.VARIO applicator for marking entire terminal strips

Time savings of up to 70 percent can be achieved with the Thermomark E.Vario thermal transfer roll printer from Phoenix Contact. The applicator is part of the new Thermomark E series. The modular system combines a powerful thermal transfer roll printer with four different applicators.

The printer marks entire terminal strips with just two materials in continuous format for tall and flat marking grooves. At the same time, the continuous material is individually tailored to the appropriate pitch. All widths between 3.5 and 1,000 mm can be realized, regardless of the number of different pitches. The perforations are assigned automatically based on the data from the engineering software.

Thanks to the automated process, the new system offers easy handling and ensures the consistently high quality of terminal strip markings.

Press Contact
Eva von der Weppen | Corporate Communications