Switzerland relies on solar
Project goal
In Switzerland, they are using a retrofit system of lightweight photovoltaic panels on the roof of an existing building to harvest energy from the sun for auxiliary power consumption.
Milestones
- 47,500 kWh yield per year
- Investment of more than 140,000 CHF
System performance
Photovoltaic area
Photovoltaic offensive on the roof
In Switzerland, they show you how it’s done: Making the roofs of existing buildings fit for the energy revolution. Phoenix Contact AG in Tagelswangen has invested a good 140,000 CHF in order to harvest solar power on the roof of the company building located northeast of Zurich.
Embedded in intelligent building technology
This measure to improve climate protection is simple and effective at the same time. A look at the construction log shows that the entire project was completed in just a few weeks. The work started with checking the seal of the existing roofing material before proceeding with the installation of the panels and the erection of a weather station. In terms of networking, the photovoltaic roof is integrated into the technical building utilities (TBU) via the Emalytics building management system from Phoenix Contact – including measurement data acquisition and visualization of the operating data on a dashboard.
Connect with us
This might also interest you
Brazil tackles social disadvantages
The company in Greater São Paulo provides broad-based vocational training for nine young people from poor backgrounds – with enormous social impact.
China harvests solar energy
With a new photovoltaic system, Phoenix Contact China is investing in self-supply using renewable energy.
Germany hosts a rally
Extensive program for the workforce brings sustainability to life.