Manually
What you will find in this section:
The digital output complies with IEC 61131-2 Type 3. It can be configured via the web server or the Modbus communication interface.
Manually
With the “Manually” function, the digital output can be enabled and disabled via the Modbus communication interface. Here, you also have to define whether the output is normally closed (NC) or normally open (NO) in idle state.
|
Navigation on the web server |
“Settings, Digital output”, “Manually” function |
|
Status |
The “Status” area shows the current status of the digital output. |
|
Identifier |
The identifier can be used to assign a user-specific designation to the digital output. |
|
Idle level |
There are two possible statuses for the idle level. – NC: Normally closed – NO: Normally open The default setting for the digital output is NO. |
Related topics