Digital Output
What you will find in this section:
The digital output complies with IEC 61131-2 Type 3. It can be configured via the web server or the Modbus communication interface.
Digital output
|
Navigation on the web server |
“Settings, Digital output” |
|
Status |
The “Status” area shows the current status of the digital output. |
|
Identifier |
The identifier can be used to assign a user-specific designation to the digital output. |
|
Idle level |
There are two possible statuses for the idle level.
The default setting for the digital output is NC (normally closed).
Only one function can be configured at a time.
The digital output is deactivated by default. |
Related topics