Deactivating the Digital Output
What you will find in this section:
The digital output complies with IEC 61131-2 Type 3. It can be configured via the web server or the Modbus communication interface.
Deactivating the digital output
The digital output can be deactivated, so that no function is assigned to it.
|
Navigation on the web server |
“Digital output, Settings“, “Deactivated” function |
|
Status |
The “Status” area shows the current status of the digital output. |
|
Settings |
Set the digital output according to your requirements. |
|
Identifier |
The identifier can be used to assign a user-specific designation to the function. |
|
Idle level |
There are two possible statuses for the idle level.
The default setting for the digital output is NO. |
|
Function |
Select the “Deactivated” function from the drop-down menu. |