Device Status
What you will find in this section:
The digital output complies with IEC 61131-2 Type 3. It can be configured via the web server or the Modbus communication interface.
Device status
The “Device status” function can be used to check whether the device is on or off.
Here, it is also possible to define whether the output is normally closed (NC) or normally open (NO) in idle state.
|
Navigation on the web server |
“Settings, Digital output”, “Device status” function |
|
Status |
The “Status” area shows the current status of the digital output. |
|
Identifier |
The identifier can be used to assign a user-specific designation to the digital output. |
|
Idle level |
There are two possible statuses for the idle level.
The default setting for the digital output is NO. |
Related topics