Tariff Selection
What you will find in this section:
The digital input complies with IEC 61131-2 Type 3. It includes the following functions:
- Impulse counter
- Tariff selection
- Synchronization of average values
- Acknowledgment of alarms
Tariff selection
A switchover from one tariff to another can be performed via the digital input. Depending on the status of the input signal, tariff meter 1 or tariff meter 2 is used. Two of the four tariffs of the device can be used via the digital input.
Via the web server, you can manually configure up to four tariffs (identifiers 1...4) and read them via the communication interface.
|
Navigation on the web server |
“Settings, Tariffs” |
|
Status |
The “Status” area shows the current status of the digital input. |
|
Settings |
Set the impulse counter according to your requirements. |
|
Identifier |
Define the two identifiers (names) for your tariffs. |
|
Mode |
Specify the digital input as method for using the tariff selection. |
|
Digital input |
Define the status of the digital input in relation to the identifier. |
Related topics