Synchronization of Average Values
What you will find in this section:
The digital input complies with IEC 61131-2 Type 3. It includes the following functions:
- Impulse counter
- Tariff selection
- Synchronization of average values
- Acknowledgment of alarms
Synchronization of average values
By means of the digital input, the synchronization pulse can be used for starting the respective average value generation.
|
Navigation on the display |
“UL-L, UL-L ...” |
|
Navigation on the web server //should this be split// |
“Settings, Average values” |
The digital input can be used to synchronize the average value generation. This function is used, e.g., when energy requirements have been defined that are not to be exceeded.
When the average values are not synchronized, the measuring results might not correspond to the relevant energy requirements.