Digital Input
What you will find in this section:
The digital input complies with IEC 61131-2 Type 3. It includes the following functions:
- Impulse counter
- Tariff selection
- Synchronization of average values
- Acknowledgment of alarms
Digital input
|
Status |
The “Status” area shows the current status of the digital input. |
|
Linked functions |
The digital input has been configured with a defined function. By clicking the respective link, you can access the configuration page for the function. |
|
Settings |
An identifier can be assigned to the digital input. With the checkbox, it can be activated or deactivated. In the default settings, the digital input is activated. |
Related topics