Impulse Counter
What you will find in this section:
The digital input complies with IEC 61131-2 Type 3. It includes the following functions:
- Impulse counter
- Tariff selection
- Synchronization of average values
- Acknowledgment of alarms
Impulse counter
The impulse counter counts the pulses generated by an external device.
It is possible to assign a measuring unit (volume, weight, distance, electrical power or an own unit), as well as the valency.
|
Navigation on the web server |
“Settings, Impulse counter” |
|
Status |
The “Status” area shows the current status of the digital input. |
|
Settings |
Set the impulse counter in accordance with your requirements. |
|
Activate |
The impulse counter can be activated/deactivated with the checkbox. |
|
Valency |
The impulse corresponds to the set value and is thus an additional multiplier. The valid value range is 1 … 65535. |
|
Unit |
Select a unit from the drop-down menu, or assign an own unit by selecting “Custom”. Unit: You can select between the following units:
You can use the “Custom” option to define an own unit. |
Related topics