Acknowledgment of Alarms


What you will find in this section:

  1. Acknowledgment of alarms
  2. Related topics

 

The digital input complies with IEC 61131-2 Type 3. It includes the following functions:

  • Impulse counter
  • Tariff selection
  • Synchronization of average values
  • Acknowledgment of alarms

 

Acknowledgment of alarms

 

In most applications, configured alarms that occur in the event of an error in the application are self-acknowledging. After the error status has been restored to the normal status (operation) of the applications, the alarm message disappears again.


You can save an error status in the application until it is manually reset via the digital input.

 

 


EMpro online documentation
Published/reviewed: 2025-07-15, en revision 003Version history