Selecting, Copying, Moving, and Deleting Elements
The following sections describe the various operations that are common to all elements visible in the workspace. You can use these functions as a reference for performing operations with elements.
| Further Info
For procedures that are specific to an element, see the relating information in the "Inserting and Editing Elements/Products" topic. |
This topic contains the following sections:
Selecting/deselecting elements
| To... | Do the following... |
|---|---|
| Select a single element | Click the element in the workspace. |
| Select all visible elements | Press <Ctrl + A>. (Selection excludes mounting rails.) |
| Select several elements by dragging | Position the cursor outside the elements and drag out a rectangle around all the elements you want to select.You can use the buttons for element selection mode in the upper right corner to define how elements are framed during mouse selection. |
| Select several elements by clicking | Hold the <Ctrl> or <Shift> key while clicking the elements you want to select. |
| Deselect an element | Hold the <Ctrl> key while clicking the elements you want to deselect or press <Esc>. |
Currently selected elements are highlighted in yellow. Exception: If you select a mounting rail, the mounted elements are not highlighted, but they are always moved together with the rail.
Copying and pasting elements
| To... | Do the following... |
|---|---|
| Copy and paste by shortcut | Press <Ctrl+C> to copy the selection to the clipboard, then press <Ctrl+V> to paste the selection in the workspace.In the workspace, the copied object will be placed right to the selected object (see the note below). |
| Copy and paste by dragging | Keep the <Ctrl> key pressed while dragging the mouse cursor. |
| Copy and paste via the radial menu | Right-click the selection and click the Copy button in the radial menu, then right-click another object and click the Paste button in the radial menu. |
| Note
You can select an item on the mounting rail before pasting in order to define the position of the copy. The copy is placed to the right of the selected object. If you deselect the copied object after copying, the object is added to the mouse cursor. You can then place the object at any valid position by left-clicking the mouse button. |
- To another position on the mounting rail.
- Between mounting rails and mounting plates.
- Between projects.
Moving elements
| To... | Do the following... |
|---|---|
| Move element(s) | Hold down the left mouse button as you drag the selection to the new position. |
| Move elements along the mounting rail ruler | Keep the <Shift> key pressed while dragging the selection on the mounting rail, The element "snaps in" with the measurement steps (lines) that are currently visible for the rail ruler. The more you zoom in, the smaller the steps the element is moved (max. 1/10 mm). |
- To another position on the mounting rail.
- Between mounting rails (or complete mounting rails between plates).
- From the Insertion Center to the workspace or to the Unplaced Elements window.
Deleting elements
| To... | Do the following... |
|---|---|
| Delete by shortcut | Press <Del> to delete the selection. |
| Delete via the radial menu | Right-click the selection and click the Delete button in the radial menu. |
| Delete via project tree | Activate the check box(es) for the objects to delete and press <Del>. |