The content you are viewing is tailored for Saudi Arabia. View Content for United States | Choose Another Country

The right choice with the new online configurator for system cabling for controllers

2025-06-24
System cabling online configurator

The new online configurator for system cabling for controllers from Phoenix Contact supports the quick and easy selection of a tailored system cabling solution.

The intuitive user interface and 3D models ensure that the new tool is easy to use. With just a few clicks, you can select your solution components consisting of front adapters, system cables, and signal transfer modules. A product selection can be immediately displayed as a 3D model for visual feedback.

Once the individual system cabling solution has been selected, a solution ID is automatically assigned, which can be called up again on the website if required. The PDF file that is also generated describes the solution components in detail and is available for download.

Press Contact
Eva von der Weppen
Eva von der Weppen | Corporate Communications