DC grid planning. Rethinking energy.

Successful implementation begins with the right design, the right components, and experienced partners for efficient and future-proof DC infrastructures.
Discussing the planning of DC power grids

Why implement DC power grids? Sustainable, economically viable, technically feasible

DC power grids enable low-loss power distribution, increase the use of self-generated electricity, and ease the load on the AC infrastructure. They are modular, scalable, and can be flexibly integrated into existing systems. Another advantage is that the technology can already be implemented right now, as components, standards, and practical knowledge are already available.

  • Sustainable energy use: DC power grids enable the direct use of PV electricity, recuperation, and storage
  • Optimized infrastructure and costs: fewer conversion steps, lower material usage, and smoothed peak loads reduce costs
  • Future-proof system integration: scalable DC grids are ideal for integrating generators, storage systems, and loads
Three people discussing a DC power grid

Comprehensive planning of DC power grids From the source to consumption

The successful implementation of a DC power grid begins with the well-thought-out planning of all relevant system components. These include:

  • Distribution: Outline of the grid structure with clearly defined current paths and protection concepts
  • Consumption: Analysis of load profiles and integration of DC-capable loads
  • Feed-in: Determination and dimensioning of suitable energy sources
  • Storage: Selection and dimensioning of suitable storage technologies for peak shaving and security of supply

Safety-compliant installation, the appropriate selection of topologies, and choosing suitable components are key to the success of the project. The following section provides an overview of the technologies that will aid implementation. To operate your grid with direct current, please contact our planning experts.

Preview with cover page of the special edition of UPDATE on DC power grids

Working together toward a DC future Partnerships as the key to DC transformation

The successful implementation of DC power grids requires more than just technology. It thrives on strong partnerships. In the special issue “UPDATE DC power grids”, you can find out how we are actively shaping the energy transition with our partners. From planning and installation to standardization – DC is becoming a collaborative undertaking.

What’s involved?

  • The DC factory in Blomberg: energy-efficient and intelligently networked
  • DC in practice: real projects, real challenges
  • Safety tests: short-circuit tests with 10 kA – safe and visible
  • Innovations: ArcZero and ELR HDC for safe connection and switching
  • DC experts: passionate about the All Electric Society

This issue is a must for anyone who wants to understand, plan, or use DC.

Contact

Our expert will help you outline your DC power grid.

Portrait of Tobias Lüke
Tobias Lüke
DC application expert
Based on the experience we have gained in our own production building, we will be happy to advise you on the planning and implementation of a DC power grid.