Application example
2025-08-22

Consume electricity and save money The energy transition not only brings challenges, but also enormous opportunities. The All Electric Society Factory in Blomberg, Germany, demonstrates how battery storage systems and DC grids are ushering in a new era together. A project with a lighthouse effect.

Open storage container with Roman Alberti, Michael Freudel, and Tobias Lüke
Tobias Lüke (Phoenix Contact) discussing the integration of PV systems and energy storage systems into local DC grids with Roman Alberti and Michael Freudel from Voltfang

The need for flexible storage solutions is increasing with the growth of renewable energies

Dynamic electricity market

389 – this is the number of hours with negative electricity prices in Germany in the first half of 2025. An all-time record, not only nationally but worldwide. “Above a renewable energy share of 50 to 60% in the electricity mix, storage systems become increasingly important. Otherwise there will be even more days with negative electricity prices”, says Roman Alberti, General Manager of Voltfang GmbH. The idea seems crazy: there are days when electricity consumers with dynamic electricity tariffs receive money for consuming electricity. But this is exactly what happens when prices on the electricity exchange are negative.

Conversely, electricity prices can skyrocket during periods of darkness. While Scandinavian countries are able to balance out strong fluctuations well with hydropower and pump storage, the electricity market in Germany currently is particularly dynamic. The same applies to all countries with a high proportion of weather-dependent electricity generation such as wind and solar power.

Michael Freudel and Roman Alberti from Voltfang standing in the battery storage system container

Tobias Lüke from Phoenix Contact (left) with Michael Freudel and Roman Alberti from Voltfang

Energy storage systems as a business model

One challenge that electricity producers and grid operators have had to face has led to a veritable gold rush in the field of energy storage. Companies are investing heavily in battery storage systems in order to buffer electricity and feed it into the grid in a targeted manner – a lucrative business area. The treasure hunters in the gold rush are already queuing up at the German Federal Network Agency, the Bundesnetzagentur. They want to stake their claims and are vying for grid connections.

However, this turbulent situation is also a great opportunity. “We can export business models abroad because this situation affected us earlier than others”, Roman Alberti is convinced. His company, Voltfang GmbH, specializes in sustainable battery storage systems made from used e-vehicle batteries. “We will need much more energy storage to ensure grid stability in Europe”, he adds. Germany can play a pioneering role in the orchestration of stable grids similar to the role Norway played in the field of e-mobility.

In the DC factory

The stability of the energy grid is not only of great significance for the large electricity suppliers. “We have to make industry as independent as possible, with PV systems, direct current grids in the factory, and, on the other side, we have to smooth out the fluctuations”, continues Alberti.

An intelligent energy management system, renewable energies, battery storage systems, and direct current solutions: These are pieces of the puzzle that together protect industry from high electricity prices. At the All Electric Society Factory in Blomberg, Germany, these pieces of the puzzle have been put together to form a coherent picture: solar panels shine across 11,000 square meters of roof space, the production machines work on the DC power grid, and a large container with a battery storage system and DC charging stations stand in front of the building.

View of the production hall in the All Electric Society Factory

The industrial DC power grid is at the heart of the All Electric Society Factory in Blomberg, Germany

Greater efficiency with direct current

“A DC power grid optimizes the entire energy chain, from generation, through distribution, right through to consumption”, explains Tobias Lüke, Phoenix Contact’s DC power grid expert. This not only avoids conversion losses. DC grids in combination with battery storage systems take peak loads out of the system. This becomes particularly relevant in the face of volatile electricity markets and fluctuating feed-in levels.

The DC factory in Blomberg, Germany is a showcase example of sector coupling in action. It demonstrates the intelligent interconnection of electricity generation, storage, distribution, and consumption across different working areas. “The industrial DC power grid is the heart of the All Electric Society Factory in Blomberg, Germany”, summarizes Tobias Lüke.

View of the Voltfang storage container in front of the All Electric Society Factory

View of the Voltfang storage container in front of the All Electric Society Factory

Integrating battery storage systems into the DC power grid

Although battery storage systems absorb direct current, they have so far almost exclusively been integrated into conventional AC power grids. Direct integration into direct current grids is technologically complex and has barely been tested to date. “Together with Voltfang, we have managed to implement a battery storage system coupled via a DC power grid that absorbs surplus energy from photovoltaics”, reports Lüke. This energy then is then fed back into the production process. With this approach the cooperation partners were able to increase the overall stability of the system. “The biggest challenge in integrating the energy storage system was the control technology. This technology enables the battery storage system to be used optimally in the DC power grid and adapted to all usage scenarios”, reports Michael Freudel, Development Engineer at Voltfang.

View into the Voltfang storage container in front of the All Electric Society Factory

View into the Voltfang storage container in front of the All Electric Society Factory

Sustainable battery storage systems made in Germany

Another aspect of sustainability is the use of second-life batteries from electric vehicles. “Only a few of the raw materials that we need for battery production are produced here in Europe”, explains Alberti. “This makes it all the more important that we make efficient use of the resources that are already available in the country”.

The battery modules come from renowned car manufacturers, either as second-life batteries or from production surpluses. Because standards in the automotive industry are very high, these batteries have an unusually long service life. “We also carry out intensive monitoring: every 10 seconds we check how the individual battery cells are behaving. This ensures a service life of 15 years and longer”.

Tobias Lüke testing the power electronics in the DC factory’s energy storage container

Tobias Lüke is Phoenix Contact’ DC expert

DC grids and battery storage systems in harmony

Michael Freudel emphasizes how well modular energy storage systems like these can be adapted. “The entire energy management system is much more flexible. In addition, the intelligence of the energy storage systems means that sector coupling can easily become reality“.

The DC power grid runs through the All Electric Society Factory like the fine network of veins running through our bodies. It not only supplies every cell with fresh energy, but also absorbs surpluses. “The advantages are obvious: we have fewer conversion losses, increased overall system stability, and we use fewer resources”, summarizes Tobias Lüke.

“Battery storage systems and direct current technology simply belong together. They are absolutely key technologies on the way to the All Electric Society”.

The All Electric Society Factory in Blomberg, Germany

Direct current flowing through a fine network of wires in the All Electric Society Factory

Summary: Fit for the future

The energy transition is not a distant goal – it has been taking place for a long time, both in large supply grids and decentrally in factories and residential areas. The All Electric Society Factory in Blomberg, Germany, demonstrates how companies can respond today to the challenges of tomorrow: with intelligent energy storage systems, DC grids, and renewable energies. Investing in such solutions now makes you less dependent on the volatile electricity market, reduces costs in the long term, and strengthens your own competitiveness.

Author: Iris Schaper

E-Mail:
Free on-demand webinar
DC power grids: From the concept to reality

Everyone is talking about direct current. But how does the technology work in practice? How big is the savings potential? What hurdles are there and how can they be overcome? Tobias Lüke, a Phoenix Contact expert, explains the basics and describes the implementation using specific examples.

Register now
Tobias Lücke, DC Phoenix Contact expert

Connect with our experts

“We will be happy to advise you on the All Electric Society and sector coupling”.

More posts