-

Data Exchange with MARKING system

You can export (transfer) all labels used in cxE with content to MARKING system and, for example, directly activate the print process in MARKING system. Once you have started the export in cxE, one or several MARKING system projects with all labels are automatically created for further processing. The number of MARKING system projects that will be created depends on the data transfer mappings configured for the Universal Data Interface (UDI) (see below).

This topic contains the following sections:

Software requirements

The following software must be installed prior to the transfer of label data from cxE to MARKING system:

Workflow

In order to start the export process from cxE, select INTERFACES >  EXPORT | MARKING system. When the export is started, the following steps are executed:

  1. A connection to MARKING system is automatically established, the UDI service is started in MARKING system and MARKING system is connected to the UDI service. (The connection is closed when you exit MARKING system.)

    The UDI status icon appears in the upper-right corner of the MARKING system's menu bar when the UDI service is running.

    Note
    The UDI service must be running for the data exchange process. If it's not, manually start the UDI service by clicking the INTERFACES > Universal Data Interface | UDI Start button in the ribbon of MARKING system or by pressing the Start service button in the INTERFACES > Universal Data Interface | UDI Settings dialog.

  2. Depending on the process settings configured for the UDI (see below), MARKING system opens with the project(s) created from the export data, the project(s) are printed directly, and/or the data is saved in a project file.
  3. The UDI configuration web page is opened in your default web browser (see the following section).

Universal Data Interface (UDI) configuration

The Universal Data Interface (UDI) is part of MARKING system. The interface is used for the transfer of the label data from cxE to MARKING system. The UDI configuration web page is automatically opened in your default web browser when you start the export.

Note
You can manually open the UDI configuration web page by clicking the INTERFACES > Universal Data Interface | UDI Start button in the ribbon of MARKING system.

UDI configuration web page

The UDI configuration web page provides the following areas: