The content you are viewing is tailored for Australia. View Content for United States | Choose Another Country

Extension of the safety portfolio – safe I/O modules for Failsafe over EtherCAT

2024-02-20
Safe I/O module

To implement a safe system, Phoenix Contact offers two new safety I/O modules for Safety over EtherCAT (FSoE) in a compact design.

Safety over EtherCAT (FSoE) has established itself as an important safety protocol alongside Profisafe. Phoenix Contact supports this market trend with the compact AXL SE family. Safety solutions based on FSoE can be implemented easily and in a space-saving way in conjunction with the EtherCAT bus coupler. The AXL SE FSDI8/3 module has eight safe digital inputs in three-conductor connection technology. The AXL SE FSDO4/2 module has four digital outputs up to 2 A.

Press Contact
Eva von der Weppen
Eva von der Weppen | Corporate Communications