Importing Configuration Data
What you will find in this section:
If you want to apply existing configurations to other devices, you can transmit the configuration data as follows:
- Exporting configuration data
- Importing configuration data
- Direct transfer of configuration data
Importing configuration data
|
Navigation on the web server |
“System, Configuration data, Import configuration“ |
If you want to load an existing configuration file onto the device, you can use the “Choose file” button to select it.
Use the “Import” button to load the selected file onto the device.