Exporting Configuration Data
What you will find in this section:
If you want to apply existing configurations to other devices, you can transmit the configuration data as follows:
- Exporting configuration data
- Importing configuration data
- Direct transfer of configuration data
Exporting configuration data
|
Navigation on the web server |
“System, Configuration data, Export configuration” |
If you want to export the entire device configuration, all checkboxes except the network configuration are enabled.
To perform a 1:1 device exchange, or to download an identical device configuration, click “Select all”. All checkboxes in the overview are enabled.
Another option is to perform a partial configuration by only enabling the required checkboxes. In this case, only the selected configuration is downloaded.
Press the “Download” button to download the configuration.