Direct Transfer of Configuration data
What you will find in this section:
If you want to apply existing configurations to other devices, you can transmit the configuration data as follows:
- Exporting configuration data
- Importing configuration data
- Direct transfer of configuration data
Direct transfer of configuration data
|
Navigation on the web server |
“System, Configuration data, Transfer configuration” |
By directly transferring the configuration data, you prevent caching on a local computer.
If you want to transfer the entire device configuration directly from one device to another, use the “Select all” button to enable all checkboxes in the overview. The network connection is not activated. If you want to include the network configuration, select it additionally.
Observe the following:
- You have to know the IP addresses and passwords of the devices.
- All devices have to be accessible via the network.
In addition to transferring the entire device configuration, you can also perform a partial transfer of the configuration by selecting the required checkboxes.
Enter the device addresses and passwords into the respective fields.
To check the connection to the entered device, click the “Check connection” button.
Click the “Transfer” button to transfer the selected configuration data to the devices.